Hi everyone, I’ve been reading through the previous discussions here regarding airflow optimization in compact 2U enclosures. One specific point that caught my attention was the mention of how standard chassis fans often struggle to maintain positive pressure when the internal drive bays are fully populated. This is exactly the wall I’ve hit with my current project.
I’m currently transitioning a data-heavy workstation from consumer-grade SATA over to an enterprise-grade storage setup. I recently integrated a few 3.2TB 2.5-inch SAS 12Gbps SSDs to handle a massive increase in simultaneous I/O streams. While the 12Gbps throughput is absolutely incredible compared to what I’m used to, the heat dissipation has been a bit of a shock. In my experience with consumer SSDs, thermals are almost an afterthought, but these 3.2TB enterprise drives seem to run significantly hotter, especially when they’re under sustained load in a tight 2.5-inch form factor.
My current setup has four of these drives stacked closely together, and even with the intake fans cranked up, I’m seeing some worrying temperature spikes that I suspect might lead to thermal throttling during long data-logging sessions. I really want to stick with the 12Gbps SAS interface because the latency is so much lower for my specific use case, but I'm worried about the longevity of the hardware if I can’t get the "hot spots" between the drives under control.
Has anyone here experimented with custom 3D-printed ducting or specific active-cooling backplanes to help move air directly across the surface of enterprise SAS drives? Or is it generally better to just sacrifice the density and leave empty slots between the drives to allow for better natural convection?
Comments