Having the best rated vacuum cleaner for home is important for many different reasons. A good vacuum cleaner won’t just keep your house clean and tidy, it will also keep you and your family safe from invisible threats like airborne bacterias and irritating allergens like fine dust and pollen. And for pet owners who regularly have to deal with pet hair, a nice vacuum will be your saving grace from those pesky hair strands that can get anywhere and everywhere.
In this article, we’ll first answer the age-old question of “What is a good vacuum” and show you exactly how you can pick up the best vacuum cleaners on the market by yourself. Next, we have a couple reviews on best vacuum cleaners for you to check out thereafter.
Picked For You: https://thekinglive.com/shark-navigator-lift-away-nv352.html
What Is a Vacuum Cleaner and Which One Is Best?
When it comes to the question of “Whats a good vacuum cleaner”, we believe that the best vacuum cleaner is a vacuum that performs well (can clean up everything on its path and on every kind of surface) but it’s also easy to maneuver, handle, and use.
- Performance
In terms of performance, most vacuum cleaners have a “floor specialty”, as in a vacuum model will perform best on a certain floor type and less effective on another. Therefore, before you even do anything, it will be wise to survey your house first.
See what kind of floor type you will have to deal with most around the house (usually, it is either hardwood floors or carpeting.)
Once you got that out of the way, pick a vacuum that works best for your home. For example, if you have a lot of hardwood floors to clean, pick one that has the greatest hard floors performance. On the other hand, if you have many carpets and rugs to comb through, consider buying the best vacuum for carpet.
Consider the type of debris you will be dealing with, too. Most vacuums will be fine with handling the ordinary dust, dirt, and debris. However, if you have to clean up pet hair, get a special pet hair vacuum.
- Ease of Use and Maneuverability
Your vacuum should, first and foremost, be easy to use. Nobody really wants to have to spend fifteen minutes reading the user’s manual to find the power button. It shouldn’t also take you a long time to figure out what all of the buttons on the vacuum does. The design of the best rated vacuum cleaners are all simple enough they can be picked up by kids and wielded expertly in five minutes max.
Lastly, maneuverability. The best vacuum cleaners in the world are super maneuverable. With them, you can weave effortlessly between furniture, reach into cramped spaces like underneath furniture and into nooks and crannies without any issue.
But you don’t really need to have the best vacuum cleaners in the world to have excellent maneuverability. Many affordable vacuums can offer that along with high performance, too.
Here we have a list of a few of them.
Dyson V11 Outsize
The Dyson V11 Outsize is our answer to the question: “What is the best rated vacuum cleaner”
Dyson is a huge name in the vacuum cleaning industry and not without a good reason: their product almost always meets expectations. With the V11 Outsize, though, Dyson has exceeded the expectation of many, including us.
In comparison to the normal Dyson V-series vacuum, the V11 Outsize has an extra large dust cup and a cleaning head that’s almost doubled the size of a standard head. As a result, you will be able to clean a much wider area of your house’s floor with each sweep. Additionally, the generously-sized dust cup will allow you to clean for longer without having to empty it.
The vacuum allows you to fine-tune its performance with three different cleaning modes: Eco, Auto, and Boost. Depending on the kind of debris you’re dealing with and the floor type of your home, you can set up your vacuum for most optimum performance. But our recommended cleaning mode must definitely be the Auto Mode. In this mode, the vacuum’s computer takes control of everything, from the suction to the brush roll speed. The vacuum has numerous smart sensors on-board to figure out what kind of performing level it needs to best clean out the home. All you really have to do is to push it around until the whole house is cleaned!
We’re highly impressed by the way the V11 Outsize can clean in our test. It can handle hard floors with no problem and even the thickest carpets and rugs we could find didn’t seem to faze it. In fact, it is probably the best vacuum for carpet we’ve had the opportunity to test yet.
Overall, an excellent purchase if you’re looking for a nice vacuum to buy.
Shark APEX AZ1002
The Shark APEX AZ1002 offers nearly the same performance level as the Dyson V11 Outsize at a fraction of the price. The vacuum performs excellently in all of our tests on hard floors and carpeting. According to our testers and many of the customers we interviewed, the vacuum is also remarkably quiet for the kind of pure cleaning performance it can dish out.
The APEX AZ1002, like many premium Shark vacuums, has a Lift-Away canister. The canister can be detached from the rest of the vacuum and you can use it to clean out problematic places like the ceiling, countertops, or shelves. Just press the Lift-Away button on the AZ1002’s body and you’re good to go.
We also like the filtration technology available on the AZ1002. It has Anti-Allergen Complete Seal technology which essentially seals up all of the seams and cracks on the vacuum’s body to prevent microscopic dirt particles from escaping. It also has a HEPA filter— the best type of filter all around— for better particle-trapping efficiency.
Miele Complete C3 Vacuum for Soft Carpet
The Miele Complete C3 is a multi-talented canister vacuum. It can clean out dust, dirt, and debris on hard floors just as well as it cleans out plush carpeting and rugs.
The key to its extraordinary cleaning performance isn’t just the strong suction motor hidden inside of its compact body. It is also the power nozzle with a small (but incredibly strong) motorized brush roll. Better yet, the brush roll has five adjustable levels for you to calibrate its performance in accordance to the height and denseness of your carpet’s piling. Do this well enough and every carpet and rug of yours can be cleaned out in short order by the Complete C3.
And as for maneuverability … there’s not much to say. Canister vacuums are among the most maneuverable and compact type of vacuum out there. You will love the Complete C3 if lightweight, compactness, and maneuverability are what you root for in a best vacuum cleaner for home.
The vacuum is equipped with a HEPA filter, so if your house has allergy sufferers, this vacuum will be perfect.
Conclusion
We hope that with this best vacuum cleaners reviews, you will have found a great, new vacuum to spend your money on! We assure you that whichever vacuum you choose on our list, you will come to love them after a while.
But in case you haven’t, don’t worry. We still got many more reviews on the best vacuum cleaners for you to look through on our site.