How do you feel about this article? Help us to provide better content for you.
Thank you! Your feedback has been received.
There was a problem submitting your feedback, please try again later.
What do you think of this article?
In response to rising fuel prices and Government-mandated emissions controls, the number of pure electric and plug-in hybrid cars on the world’s roads accelerate to over 5 million by the end of 2018, according to analyst EV-Volumes. This rapid growth in production volumes is being matched by equally rapid advances in powertrains, power electronics and battery technologies.
These advances also highlight the increasingly critical role played by a previously unsung vehicle component: the DC/DC converter. Irrespective of whether a car is a pure EV or a hybrid, DC/DC voltage conversion is at the heart of its power electronics systems.
The converter is fundamental to the overall efficiency and performance of electric and hybrid vehicles for several reasons:
- The flow of power between the HV and 12 V buses is bi-directional and can change in milliseconds according to the demands of the vehicle’s systems and driver input so large loads must be converted seamlessly and safely for smooth, predictable vehicle operation.
- Because of the high electrical loads they carry, most DC:DC converters are water-cooled, which adds weight and costs when installed in the vehicle. There is strong pressure to simplify this, to minimize cooling requirements, cut weight, and improve efficiency.
- The converter must be robust enough to continue to operate efficiently across a wide range of environmental and driving conditions.
Given the pace of development of vehicles, and the constant pressure to keep costs down across the test and development lifecycle for converters, efficient simulation, design, validation, and manufacturing testing of the converters is essential. However, this presents its own challenges.
Converter testing challenges
The design and test obstacles result from many factors:
- Bi-directional test: Testing bi-directional power flow demands equipment that can both source and sink power to the converter. But conventional test methods using external circuits and multiple instruments typically don´t allow for smooth signal transitions between sourcing and sinking power and give inaccurate simulations of operating conditions. It also leads to excess heat build-up in the test environment.
- New power semiconductor technology: Designers are starting to use Wide Bandgap (WBG) devices, while these have some advantages, their use complicates the simulation and design of DC:DC converters. Users need to evaluate each device to determine if the WBG devices will work in their designs.
- Reliability and safety concerns: Using new semiconductors means extra validation and reliability testing is needed to ensure converters will last in harsh operating conditions. Also, given the power levels used with converters, testers need to be careful when testing them. This requires special safety mechanisms in manufacturing, including redundant systems that do not expose the tester to high voltages if a failure occurs.
- Maximizing efficiency: Because of the various operational and environmental influences on efficiency, it’s difficult for testers to simulate these to evaluate the real-world, whole system operation of the converter. Also, measuring small percentage changes in efficiency demands instruments with high dynamic range.
Converting challenges into solutions
To address these design and test issues, Keysight has developed and introduced new, innovative approaches that help manufacturers accelerate their programs. For example, high-frequency enabled simulators can accurately simulate the behaviour of new WBG semiconductors, helping to improve the efficiency of DC:DC converter designs.
New, fully integrated source/sink solutions enable more accurate simulation and testing of DC:DC converters’ transitions in power flow direction during acceleration and regeneration. These test solutions also feature the ability to return clean power to the test lab’s AC mains, reducing regenerative heat and dramatically cutting the need for costly HVAC equipment in the test system environment.
Find out more about how Keysight enables more accurate and efficient testing of the systems at the heart of the electric and hybrid vehicle revolution here.