DesignSpark Electrical Logolinkedin
Menu Search
Ask a Question

Simulating Electromagnetic Interference for the Real World

There is a dark, even destructive, force within electronics.  You can't see it, you can't touch it, but every electronics engineer needs to worry about it.  This nemesis is electromagnetic interference.

Electromagnetic interference can be the biggest headache of any electronic design.  An engineer must take care to ensure that a design does not generate unwanted interference that might affect other devices and, at the same time, is immune to interference from outside.  Clever design of electronic devices, along with adequate shielding, can help address both problems.  However the proof of the pudding is in the eating.   In other words, the only guaranteed way to make sure the design has succeeded is to make one and test it!

Image

 

 

 

 

 

 

 

 

Image:  Rainford EMC Systems

Electromagnetic Compatibility (EMC) testing is quite an involved task.  It requires a testing chamber that isolates the equipment from oustide interference and some quite sophisticated kit to measure the results.  These test chambers aren't too common and time within them can be quite expensive.  Plus what if the test fails?  A return to the drawing board and yet more testing time.  This potentially endless cycle of re-design and re-test can become incredibly expensive and time-consuming.  But there may be another way...

I have recently found out about a virtual EMC simulation service.  KEC Limited in the UK have spent over 30 years providing high-performance shielding devices to the industrial, defence and research industries.  They have just completed a two year project with the University of Reading to create a simulated environment to allow virtual EMC testing of cable harness systems which connect electronic systems together.   

Image

 

 

 

 

 

 

 

 

Image:  KEC Limited

The service that KEC offers is aimed at these external connections that devices need in order to link to the outside world - often a weak-point in any EMC system.  But simulation can only be a usable tool if the simulated results mirror the real world.  KEC are continuing to evolve the system and are currently interested in finding partners to broaden the range of their results.  If you have something you can offer, or a particularly thorny EMC problem you need to solve, drop us a line.  You may be able to contribute to a new revolution in testing techniques...

Connector Geek is Dave in real life. With 28 years in the industry, Dave likes talking about connectors almost as much as being a Dad to his two kids. He may still be a kid at heart himself...

23 Mar 2012, 12:40

Comments

May 21, 2013 07:10

Am tring to make a pcb of picaxe 28 board am not sure if my design is correct.. The thin yellow lines are the ones which i will connect on back of the board using wires so that i wont need to make a second layer.. nd i would like to place i2c chip to it,but thats nt important.. [attachment=0:1sdi85ee]picaxe 28.jpg[/attachment:1sdi85ee].I have also added a pcb pic which i have used to make my pcb[attachment=1:1sdi85ee]IMIM board 1.jpg[/attachment:1sdi85ee]

0 Votes