How do you feel about this article? Help us to provide better content for you.
Thank you! Your feedback has been received.
There was a problem submitting your feedback, please try again later.
What do you think of this article?
Not too long ago engineers would need to carry around a range of instruments to perform installation tests, but this can all be done with a multifunction testers, that will save you time and money – One tester negates the need of switching meters between tests (speeds up testing) and generally a single multifunction tester will be much cheaper than combined costs of the individual meters needed to perform the tests.
Now let’s take a quick look at the Multifunction Installation Tester (144-5338) :
The tester is gimmick-free, but ruggedly constructed and is the perfect solution for troubleshooting, commissioning and ensuring fixed wiring is safe and correctly installed, but as well as saving time and money the RS Pro installation tester has the following key benefits / features:
- Large selection knob to clearly show the selected function
- 5” TFT colour LCD display – wide viewing angle for easy and safe reading
- Easy to use and read menu
- Rugged construction
- Performs the following Tests:
- Insulation resistance
- Earth resistance
- Loop impedance
- Voltage - Select measurement between L-N, L-PE and N-PE
- RCD – with variable current mode for customized settings and PASS/FAIL indication
- PFC - Prospective Earth Fault Current
- PSC – Prospective Short Circuit Test
- Single readings can be captured or using datalog function results can be saved at a pre-set interval and then can be either viewed on the meter or downloaded to a PC.
- Supports
- SD memory
- USB
- Bluetooth interface