Skip to main content

Review of top programming languages for software engineers

Here is a brief review of the most popular coding languages that are used by software engineers.

C programming language is a general-purpose, imperative computer programming language, supporting structured programming, lexical variable scope and recursion, while a static type system prevents many unintended operations. By design, C provides constructs that map efficiently to typical machine instructions, and therefore it has found lasting use in applications that had formerly been coded in assembly language, including operating systems, as well as various application software for computers ranging from supercomputers to embedded systems.

C++ is a general-purpose programming language. It has imperative, object-oriented and generic programming features, while also providing facilities for low-level memory manipulation.

C# is a multi-paradigm programming language encompassing strong typing, imperative, declarative, functional, generic, object-oriented (class-based), and component-oriented programming disciplines.

Objective-C is a general-purpose, object-oriented programming language that adds Smalltalk-style messaging to the C programming language. It was the main programming language used by Apple for the OS X and iOS operating systems, and their respective application programming interfaces (APIs) Cocoa and Cocoa Touch prior to the introduction of Swift.

LPC is an object-oriented programming language derived from C and developed originally by Lars Pensjö to facilitate MUD building on LPMuds. Though designed for game development, its flexibility has led to it being used for a variety of purposes, and to its evolution into the language Pike.

Perl is a family of high-level, general-purpose, interpreted, dynamic programming languages. The languages in this family include Perl 5 and Perl 6.

Verilog is a hardware description language (HDL) used to model electronic systems. It is most commonly used in the design and verification of digital circuits at the register-transfer level of abstraction. It is also used in the verification of analog circuits and mixed-signal circuits, as well as in the design of genetic circuits.

Pascal is an imperative and procedural programming language, which Niklaus Wirth designed in 1968–69 and published in 1970, as a small, efficient language intended to encourage good programming practices using structured programming and data structuring. A derivative known as Object Pascal designed for object-oriented programming was developed in 1985.

Java is a general-purpose computer programming language that is concurrent, class-based, object-oriented, and specifically designed to have as few implementation dependencies as possible. It is intended to let application developers "write once, run anywhere" (WORA), meaning that compiled Java code can run on all platforms that support Java without the need for recompilation. Java applications are typically compiled to bytecode that can run on any Java virtual machine (JVM) regardless of computer architecture. As of 2016, Java is one of the most popular programming languages in use, particularly for client-server web applications, with a reported 9 million developers. Java was originally developed by James Gosling at Sun Microsystems (which has since been acquired by Oracle Corporation) and released in 1995 as a core component of Sun Microsystems' Java platform. The language derives much of its syntax from C and C++, but it has fewer low-level facilities than either of them.

The first step in becoming a programmer is to choose the right IT career path. Then, start learning one or two coding languages and practice them.  Read Comprehensive Review of Coding and Computer Programming article to learn more on history and evolution of programming.

Matt is founder of High School Technology Services, DC Web Makers and Coding Bootcamps. He has written extensively on advance topics on web design, mobile App development and blockchain. He is a senior editor at Touchstone Words where he writes and reviews coding and technology articles. He is also senior instructor and developer living in Washington DC. You can follow him on Linkedin.