Skip to main content

Raspberry PI and Arduino in industrial environments

by Designerz (No longer a member)

Raspberry PI and Arduino boards are the most famous devices for rapid electronic prototyping and DIY home applications. However, their capabilities and flexibility are still largely under estimated in the industrial environment.

title

Raspberry PI and Arduino flexible programming, customizable signal types and easy adaptation to the existing installations can offer many benefits to the industrial world.

For instance, they could be great low cost and flexible alternatives to the usual industrial devices for adding remote control and monitoring functionality to small legacy industrial systems.

The 3 most common concerns about the use of such development boards in the industrial environment are:

  • Robustness in industrial environments
  • Safety
  • Industrial standard communication protocols

Robustness in industrial environments

titleThere are already several ruggedized versions of Arduino and Raspberry available in the markets.

Hardware like the

Industrial Shields Arduino based PLCs and Raspberry based panel PC provide already include the extra robustness needed to meet industrial needs.

Alternatively, there are various industrial standard enclosure specifically developed to accommodate the two boards.

Case study – Video - Blasting Robot 

Blasting robot fully automated and remotely controlled with Industrial Shields, Arduino based, PLCs.

 

Case study -  Multisensory Retail management system with Raspberry PI

Multisensory Retail management system for audio, video, lighting and fragrances synchronization developed by TairolRadio for the San Siro football stadium in Milan (A.C. Milan and Internationale football clubs)

 

Safety

This is probably the most controvert and discussed topic in Internet: Are Raspberry and Arduino boards, and related based hardware, safe solutions for the industrial applications? There is not a simple answer, it depends by many factors and require for sure a change in the mind-set of the engineers.

The safety of an industrial application does not only depend by the PLC; It always matter of the integrity of the full project, how the systems and software are implemented and how the safety have been considered when designing the project.

Here an interesting debate between engineers that approach this topic for different angles

Case study – Fortaps automated their production plant with Industrial Shields, Arduino based, PLC

Industrial standard communication protocols

This is where the flexibility of Arduino and Raspberry PI comes over.  Modbus foundation has developed specific libraries to allow the two boards to communicate via their protocol.

Modbus is a serial communications protocol developed by Modicon (acquired by Schneider Electric) for its programmable logic controllers (PLCs); it has become the most common and adopted by many automation manufacturers such as Omron, Opto 22, Schneider and Mitsubishi.

The main reasons for the wide adoptions of Modbus in the industrial environment are:

  • developed for industrial use
  • royalty-free and open published
  • easy to use, install and maintain
  • few restrictions on vendors

Modbus allows many different devices, connected to the same network, to communicate together regardless the OEMs. The needs of putting in communication different devices from different manufacturers has become even highly important with the arrival of  4th industrial revolution; The Industry 4.0 and the Industrial IoT have given a second childhood to Modbus.

Hereafter to example of Arduino and raspberry PI applications running Modbus

Video - Raspberry PI and Modbus

 

Video - Arduino and Modbus

 

The following articles show how to remotely control HVAC systems by using Arduino based hardware and SCADA.

title

SCADA

(Supervisory Control And Data Acquisition) is another industrial system for remote monitoring and control that operates with coded signals over communication channels (using typically one communication channel per remote station). The SCADA library for Arduino are openly published as well. 

Remote control of a HVAC system via Arduino based PLC

Conclusions

Arduino and Raspberry PI, in their ruggedized version, can be valuable and reliable alternatives to the well-established industrial devices (especially to connect to the internet of things small legacy industrial systems) pending an ad-hoc design of project to ensure safety.

 

Designerz (No longer a member)
This person is no longer a member and their bio is unavailable
DesignSpark Logo

Enjoying DesignSpark?

Create an account to unlock powerful PCB and 3D Mechanical design software, collaborate in our forums, and download over a million free 3D models, schematics, and footprints.
Create an account

Already a DesignSpark member? Log In

Comments