Skip to main content
shopping_basket Basket 0
Login

Program the IOT2000 with Arduino IDE!

How2Make
3




Step 1: Setting Up Your IOT2000!


You will need the next parts.
Snapshot_-_271_8fcee8efd62d1c5181b59db3e423e758ba69ed4c.png

- 9-36V DC power supply.
- Micro SD card (Min 8GB)
- 5V LED
- Micro USB cable
- Arduino IDE software

Your IOT2000 needs an SD card with the Siemens image on it.
It will boot from it.

Step 2: Create a Bootable SD Card

The next steps will explain you how to create it.
1. Place the SD card in your PC.
2. Download WIN32DiskImager.
3. Download the Siemens Image.
4. Open the WIN32DiskImager and write the file on your SD card.
Naamloos1_326b2d1022da65eb066a39f2b7ee288c453a27f7.png
5. Place it in the IOT2000. (The IOT2000 must be voltage free!)
Snapshot_-_301_9ec37b46923e2e0edd0718950199ce4e8310a47e.png



Step 3: Download the Intel Galileo Package in Arduino IDE

We must import the Intel Galileo package in the Arduino IDE software.
1. Open Arduino IDE
2. Go to Tools > Boards > Board Manager.
3. Search for "I5"
Snapshot_-_311_ed11f29b6576c2b7d597ebce98018ae3355b1687.png
4. Download & install the latest version.
5. Check at "Boards" for the Intel Galileo gen2 and select it
Snapshot_-_321_85c382d8a78c071d023a1feae02419873894e65c.png
Step 4: Power & Drivers

So we are almost there.... :)

1. Set the power on your IOT2000
2. If everything goes alright, the PWR led should be on.
Snapshot_-_331_28a1756d8c7653ab108c4fe6e9a963f18a8e93a9.png
3. It takes about 30 seconds before your IOT2000 has fully started.
4. Attach the Micro USB to your IOT2000.
5. If your PC don't reconizes your IOT2000, update the drivers manually.
6. You can download them here.


Step 5: Upload the Arduino Sketch to the IOT2000

So finally we are going to upload the Blink Sketch.
1. Open your Arduino IDE software.
2. If it's right, you should have a new COM-port named "Intel Galileo"
Snapshot_-_341_849184edce6c95724cfd43e91643ef05dadffe03.png
3. Select it.
4. Upload the Blink sketch to your IOT2000!
5. The pinlayout in the IOT2000 is the same as the Arduino UNO. (Pay attention! The Vin is the same voltage as your power supply!)
6. Attach the Led to pin 13 & GND.
7. It should be blinking! :D
Snapshot_-_351_86a950863070c19f899e5a810dd0aec84bc61384.png

How2Make has not written a bio yet…

Recommended Articles

Comments

April 10, 2017 10:37

m-scofield you are right, that library is for linkit one.
Is there a way to write an arduino ide code to publish mqtt to ubidots?

0 Votes

[Comment was deleted]

April 10, 2017 10:37

Isn't the LWifi.h a library especially for the LinkIt ONE board?
Not sure if it is possible to run it on the IOT2000..

0 Votes

April 7, 2017 09:39

Hello, i have a question, i have a code made for an linkit one board, this code uses the library wich is sending error messages when i try to compile the code to load to a iot2020 board

Ubidots_8.ino:1:19: fatal error: LWiFi.h: No such file or directory
compilation terminated.
Error compiling.

the code can be found in:
https://www.hackster.io/LSEngineering/ubidots-signal-recorder-df857b

what im trying to do is doable? where can be the problem? this only happen when i select the galileo gen2 board in arduino ide, when i change to linkit one board i dont get that problem.
Regards
LuisSalazar

0 Votes

[Comment was deleted]

[Comment was deleted]

DesignSpark Electrical Logolinkedin