How do you feel about this article? Help us to provide better content for you.

Thank you! Your feedback has been received.

There was a problem submitting your feedback, please try again later.

What do you think of this article?
In this article, I introduce two motor control applications using the RA6T1 Motor Control RSSK (Renesas Solution Starter Kit) (211-0566) .
For basic information on how to use the RA6T1 Motor Control RSSK, please refer to the following article.
Out-of-the-Box: The New RA6T1 Motor Control Starter Kit
First, let’s take a look at the procedure for dual motor control using RA6T1.
To build this environment, you will need two kits: the RA6T1 Motor Control RSSK and an additional Inverter board that includes a BLDC motor which is sold as Renesas Evaluation System for BLDC Motor (Renesas Evaluation System for BLDC Motor).
By preparing these two kits, two motors can be controlled by using one RA6T1 CPU card.
The next step is to make some modifications, such as mounting pin headers on each board so that the second inverter board can be controlled. There are basically two ways to modify it, please refer to the application note below for details.
RA6T1 Sensorless vector control for dual permanent magnetic synchronous motor Rev.1.00 - Sample Code (Note: you will need to create an account on Renesas to access this code)
Once the modifications are complete, the dual motor control is ready to be evaluated.
Next, download the sample code for the RA6T1 dual motor control from the Renesas web site and write the program. Now you can control the two motors with only one RA6T1!
In addition, by using the motor control development support tool “Renesas Motor Workbench”, you can easily evaluate the motor control by changing the motor control parameters with the GUI on your PC.
Second, I will show you the procedure for controlling a PMSM with encoder using the RA6T1.
The motor with encoder is made by Nidec Servo Corporation, and there are three steps to follow.
1) Extract the motor parameters with the Tuner function of the Renesas Motor Workbench.Write the extraction program included in Renesas Motor Workbench 2.0 distribution to the RA6T1 using Segger’s J-Flash Lite.
Next, start up the Tuner function of the Renesas Motor Workbench. When the window shows up, enter the Rated Current and Pole Pairs. This time, I entered Rated Current=1.8A and Pole Pairs=7.
This parameter is different for each motor, so please enter the information for the motor you are using.
After entering the parameters, press the Start button and wait for a while to complete the extraction of the
motor parameters. Next, click the "Output Header File" button on the right window to generate the following
file to be reflected in the sample code.
- r_mtr_control_parameter.h
- r_mtr_motor_parameter.h
Then, overwrite and save the two generated motor parameter files.
2) Set the number of encoder counts per motor shaft revolution in the configurator of the FSP.
For the motor used in this example, I set it to “1200”. This parameter is different for each motor, so please enter the information for the motor you are using.
- rm_motor_sense_encoder : Cunts per Rotation = 1200
- rm_motor_position : Encoder Cunts per one rotation : 1200.0F
3) Build and write the sample project.
The following controls can be performed in the sample code.
- Driving or Stop the motor in position control mode
- Driving or Stop the motor in speed control mode
- Change position and speed
This concludes the introduction of the two RSSK-based motor control applications. In addition, we plan to release the following sample code and application notes as a solution for RA6T1 in the near future, so please stay tuned.
- Sensorless vector control for permanent magnetic synchronous motor (1-shunt current detection)
- Block Commutation Control (Hall sensor, Sensorless)
For information to help you with your motor control design using an RA6T1 MCU, please visit:
RA6T1 motor RSSK product page: https://www.renesas.com/ra/rssk-ra6t1
RA6T1 product page: https://www.renesas.com/ra/ra6t1
RA6T1 motor RSSK introduction video: https://www.renesas.com/support/videos/ra6t1-motor-control-rssk-intro.html
RA6T1 motor RSSK setup video: https://www.renesas.com/support/videos/ra6t1-motor-control-rssk-setup.html