Skip to main content
shopping_basket Basket 0
Login
Microchip Motor Control Starter Kit Review - DM330015
pauljclarke
6

Comments

May 18, 2013 20:59

Hello again Sneuper

[quote:ag926lx9]... Why no ZENER symbol? It's a very old well known device from good old Fairchild.[/quote:ag926lx9]

Yes, that's why I corrected my post with RS 507885 which has the normal zener symbol, that you could use.

Homegirl has responed with the 3D points, you will not get a perfect 3D image, but a useful spacial awareness. You can as suggested improve your own components with the tools available.

[quote:ag926lx9]Another problem is finding a transistor, for instance your BC327-25ZL1G.
If I type BC237 in the FIND window, I do not get your transistor, but only a BC237BG. Do I have to type the EXACT type number?? Don't hope so...
Typing BC237* does'nt work. No wildchars possible??
I hate to tell you, but I am not convinced Modelsource is going to work for me. It still has a lot of dissapointing "errors" for me.[/quote:ag926lx9]

I'm not sure if your confusing the Library Manager and ModelSource here. ModelSource is a tool to select components and copy them into your local libraries. The Library Manager manages these component libraries. "FIND" is part of the Library Manager or "Add Component"
If you use ModelSource to copy the component BC327-25ZL1G into your local library (via the "Use Component" button), then "FIND" should have no difficulty in locating it.

I actually just did this to check. ModelSource instantly locates the BC327-25ZL1G using Quick Search.
In DesignSpark PCB using "Add component" and "FIND" the BC327-25ZL1G was located using contains "BC327-25ZL1G" or "BC327", without any problems.


[quote:ag926lx9]For now I will trying to use the old libraries of DesignSpark PCB and see if they work for me. ( is this possible ? )[/quote:ag926lx9] Yes, but they are unsupported, whereas ModelSource will be corrected and updated.

[quote:ag926lx9]I will keep following the Modelsource idea because the idea is nice but the implementation is not satisfying.[/quote:ag926lx9] As with DesignSpark PCB and the DesignSpark webpage, ModelSource is under a regular development and improvement plan, but obviously there is a limit to available resource for a totally free package. BUT the resource to-date has been significant.

0 Votes

May 17, 2013 07:52

As has been mentioned before on many of the threads on this forum, the 3D view is not an exact 3D representation, it's simply for space allotment. There are ways to make your 3D objects look like the device you have inserted but it means creating a new 3D model (or adding your part to one that already exists of the same format).

HomeGirl

0 Votes

May 14, 2013 21:46

Thanks for your fast reply.
I tried your transistor (BC327-25ZL1G) and YES it has a common schematic PNP transistor wat I want to see. Fine!
But still in 3D view it looks as a cubic block with no round edges as the common TO92 package has. Dissapointing...

The zener I used is a BZX79C12.
Its schematic symbol is a diode and no [u:phq7eo6v]ZENER[/u:phq7eo6v]diode symbol . Why no ZENER symbol? It's a very old well known device from good old Fairchild.
And its package shows cubic in 3D view with no wires attached . It seems to "float" above the pcb.
In fact all the components I have chosen from Modelsource appear as red or black cubic boxes in my 3D view.
And all package types I used as a test now do exist for a long time now, so why is'nt it possible to translate this directly to a good 3D package view??

Another problem is finding a transistor, for instance your BC327-25ZL1G.
If I type BC237 in the FIND window, I do not get your transistor, but only a BC237BG. Do I have to type the EXACT type number?? Don't hope so...
Typing BC237* does'nt work. No wildchars possible??

I hate to tell you, but I am not convinced Modelsource is going to work for me. It still has a lot of dissapointing "errors" for me.
And I did'nt mention very new or exotic devices in my examples, did I ?
Pitty, because a really like the design software.

For now I will trying to use the old libraries of DesignSpark PCB and see if they work for me. ( is this possible ? )
I will keep following the Modelsource idea because the idea is nice but the implementation is not satisfying.

Kind regards.

0 Votes

May 14, 2013 19:27

The zenershould have been RS 507885, sorry.

0 Votes

May 14, 2013 19:25

Hello Sneuper

Firstly have another look! ModelSource has just been updated.

[quote:g5k9o5f6]When choosing a component (PNP transistor TO92 ) from the Modelsource tab, all I get is a rectangle shematic symbol and no PNP transistor symbol.[/quote:g5k9o5f6]
Yes, some parts are as you describe, this depends on the manufacturer, however there are some work arounds to achieve what you want. For example from the ModelSource selector, select PNP and TO-92 from here you can view all the options and looking at the first in the list RS463072 has the schematic as you want. Check down the list to find one that suits your style and is accurate for your part, use it and on the schematic change the type and part number.
You could also do as above and create a new user component for the future.

[quote:g5k9o5f6]Also an ordinary zener appears as a rectangle in the schematics and has a cubic package in stead of a cilindrical package.[/quote:g5k9o5f6]
I did a quick search and all the ones I looked at had a diode symbol for the schematic, RS507873 has the more convetional zener symbol.

[quote:g5k9o5f6]Do I have to make all the symbols myself??[/quote:g5k9o5f6] It is quite easy to make or adapt symbols especially 2 or 3 pin devices. Many users/companies have their own drawing standards and do this.

[quote:g5k9o5f6]I desperately need some kind of Library tutorial, including working with Modelsource which is UP TO DATE ![/quote:g5k9o5f6]
Yes these are coming as is evident from the DesignSpark PCB home page http://www.designspark.com/page/designs ... -home-page
We are producing many updates to DesignSpark PCB and ModelSource as is evident from todays update and keeping tutorials up to date is a major task underway.
I hope this helps and encourages you to stay with this very comprehensive free package.

0 Votes

May 14, 2013 11:16

Hi,
I am a newbie starting with Designspark.
I chose to learn this software because of the many enthousiatic people out there AND its huge library.
I am learning the program pretty fast, but the libraries are very confusing and not working in my case.

The problem is that I cannot get any component nice looking in my schematics and PCB.
When choosing a component (PNP transistor TO92 ) from the Modelsource tab, all I get is a rectangle shematic symbol and no PNP transistor symbol.
The PCB footprint seems OK, but in 3D view it is an ordinary cubic block and not a TO92 package.
Also an ordinary zener appears as a rectangle in the schematics and has a cubic package in stead of a cilindrical package.
What am I doing wrong? There must be something better then rectangles I think ? Is it a program setup problem?
Where are all the thousands of prefab components? Do I have to make all the symbols myself??

I desperately need some kind of Library tutorial, including working with Modelsource which is UP TO DATE !
Some tutorials seem to be old and written for older versions.

Hope someone can help me with the libraries, its very frustrating because I like the rest of the software very much!

Thanks!

0 Votes

Related Content

DesignSpark Electrical Logolinkedin