DesignSpark Electrical Logolinkedin
Menu Search
Ask a Question
  • Home
  • Our Software
  • Mechanical software
  • when exporting to DXF when that file is opened the dimensions have changed what needs to be done ?will i have to upgrade or have i missed setting somthing up

when exporting to DXF when that file is opened the dimensions have changed what needs to be done ?will i have to upgrade or have i missed setting somthing up

0 Votes

Comments

February 12, 2020 08:57

You can check if the 'Units' are correct. Just check the scale comparison of the dimension and what it is supposed to be.
1 Inch = 25.4mm
1mm = 0.03937008 inch

0 Votes

February 12, 2020 08:57

Make sure that when you 'Save as'; In the window that opens do not tick the box to 'Overide Units'. Also make sure that the 'Units' are set to what you want. Both in DSM and the program that you want to use to open the DXF.

0 Votes