Dear all,
I'm using DesignSpark Mechanical v4.0 R19.1 2018.1.0.12131 on my desktop pc Windows 8.1
Recently when I open a project with some complexity I note that quotes of object are very slow to shown (in order of 5-6 seconds for every quote in mm)
It's quite frustrating because the objects rotation and evolution is fast
I have done some checks:
Looking on task manager there aren't problem : cpu load, ram used and time to write to disk are in normal range.
My pc have following carachteristics:
CPU Intel i5-4590S@3GHz
RAM 8GB RAM
VIDEO Shared graphic card Intel HD Graphics 4600 with 1GB of memory
HD 1TB 7200 rpm
Looking for a solution I tried this trick but with no changes:
https://designspark.zendesk.com/hc/en-us/articles/360002322918-DSM-4-0-Is-it-slow-on-Windows-10-even-with-a-high-spec-machine-
What also I can to consider in order to speed up quote visualization on objects?
Many Thanks