DesignSpark Electrical Logolinkedin
Menu Search
Ask a Question

August 19, 2019 07:30

Shell tool inside radius

I have a rectangle solid body with 1mm radius on corners, when I use the shell tool the inside corners are square.

How do I have the inside and outrside corners the same radius??

0 Votes

Comments

August 22, 2019 07:35

Corner radius has to be larger than shell thickness, ok got it.
Thanks

0 Votes

August 22, 2019 07:35

Thanks, just tried it and it works.
So the corner radius has to be larger than the shell thickness, got it. :)

0 Votes

August 21, 2019 07:28

Hi.
If the shell thickness is greater than the external blends produced from pulling edges, then the offset blend is reduced to zero and no blend is possible. In your example, shell offset less the 1mm will only produce an internal blend. Try 0.5 offset and you'll get the idea,

0 Votes