Skip to main content
shopping_basket Warenkorb 0
Einloggen

Installation problems with DSE V2.0.1


Lehrer

I would like to install the DSE on a "company PC".
also got the "OK" from the IT department too

Now it turns out that when installing DesignSparks Electrical now requires very significant admin powers.
More than DesignSparks mechanical or DesignSparks PCB.
The IT department is of the opinion that this is due to the responsible programmer
and the fact that the installation program of DSE is unstable and freezes shortly before completion, was also at the expense of the programmers of DSE.


I ask the responsible person of DSE V2.0.1 to adjust the installation routine for the program DesignSparks Electrical V2.0.1 so that only low administration rights are needed and that the installation routine does not "freeze".

With kind regards

Translated with www.DeepL.com/Translator (free version)

Teile diesen Beitrag
DesignSpark Electrical Logolinkedin