Sponsored by: RS Components
How to control ROCK GPIO with MRAA
One of the main features of the ROCK range of Single Board Computers is their input/output capability using the GPIO to control various additional hardware. Many ways exist to do this, but they tend to require expert knowledge and vary between boards.
MRAA is an Open Source project from the Eclipse Foundation that aims to make using the GPIO far easier.
In this article, I show how to use MRAA and Python to control electronics connected to the GPIO on ROCK boards. The example uses the ROCK 4C+, but it can be applied to any of the ROCK range and only requires a few components to get started.
Difficulty: Easy
Time: 1 Hr
Steps: 7
Credit: None
Licence: The MIT License (MIT) https://projects.eclipse.org/license/mit-license-mit
Step 1: Parts
Only a few easily obtainable components are required to start using the GPIO to connect to electronic devices.
You will need a ROCK board, for example the ROCK 4C+ (249-3158) .
For the breadboard test circuit, the following components are required:
- Breadboard (189-2277)
- Jumper wires (204-8243)
- Red LED 5V (228-5562)
- BS270 MOSFET (807-5184)
- 150 Ohm Resistor (707-7603)
Optionally you can run a test using just a Multimeter (123-1938)
Step 2: Installation
To follow along, you will need a ROCK board with a Debian Operating System installed. You can download the OS for your board from the Software and Downloads Hub.
MRAA is included in the Debian images so is easy to install with the following on the command-line:
sudo apt update
sudo apt install libmraa2 libmraa-dev libmraa-java python3-mraa mraa-tools
Step 3: ROCK GPIO
Each ROCK board has its own GPIO map which lays out the pin names and their functions. ROCK GPIO Headers are colour-coded to match the Pin Map to make identification simpler.
Warning: It is very important not to exceed the Maximum Voltage and Current ratings documented for each pin as this can permanently damage the board
GPIO Pin Maps along with Absolute Maximum Ratings and Notes can be found on the Radxa documentation site. For example, here’s a link to the page for the ROCK 4C+ board: https://docs.radxa.com/en/rock4/hardware/rock4-gpio
Step 4: Circuit
Build a simple test circuit on a breadboard using jumper wires with a Red LED connected to 5V via a 220 Ohm Resistor and an N-channel MOSFET (BS270).
Tip: MRAA Pin numbering refers to the physical pins on the GPIO Header, not the GPIO designation
I have chosen Pin 16 connected to the Gate of the MOSFET to control the LED. 5V power and Ground are connected to Pin 2 (5V) and Pin 14 (GND) respectively.
GPIO pins are not capable of sinking or sourcing much current so it’s good practice to use a MOSFET or BJT to protect the pins. The resistor in this circuit limits the current through the LED.
This MOSFET circuit is driven by the voltage applied to the Gate of the device and almost zero current flows through the GPIO pin it is connected to. When the pin 16 is high, the LED turns on and when it's low it is off.
If you don’t have the parts you can measure the Voltage across Pin 16 and GND with a Multimeter. You would see a voltage of about 3V when the pin is high and 0V when it’s low.
Step 5: MRAA Commands
MRAA has a command line utility mraa-gpio with various options to control the pins.
Get the MRAA Version:
mraa-gpio version
Version v2.2.0 on ROCK Pi 4
List all available pins and their functions:
mraa-gpio list
01 3V3:
02 5V:
03 SDA7: GPIO I2C
04 5V:
05 SCL7: GPIO I2C
06 GND:
07 SPI2_CLK: GPIO SPI
08 TXD2: GPIO UART
09 GND:
10 RXD2: GPIO UART
11 PWM0: GPIO PWM
12 GPIO4_A3: GPIO
13 PWM1: GPIO PWM
14 GND:
15 GPIO4_C5: GPIO
16 GPIO4_D2: GPIO
17 3V3:
18 GPIO4_D4: GPIO
19 SPI1TX,TXD4: GPIO SPI UART
20 GND:
21 SPI1RX,RXD4: GPIO SPI UART
22 GPIO4_D5: GPIO
23 SPI1CLK: GPIO SPI
24 SPI1CS: GPIO SPI
25 GND:
26 ADC_IN0: AIO
27 SDA2: GPIO I2C
28 SCL2: GPIO I2C
29 SCL6,SPI2RX: GPIO I2C SPI
30 GND:
31 SDA6,SPI2TX: GPIO I2C SPI
32 GPIO3_C0: GPIO
33 SPI2CS: GPIO SPI
34 GND:
35 GPIO4_A5: GPIO
36 GPIO4_A4: GPIO
37 GPIO4_D6: GPIO
38 GPIO4_A6: GPIO
39 GND:
40 GPIO4_A7: GPIO
Turn on the LED connected to pin 16 then turn it off again:
mraa-gpio set 16 1
mraa-gpio set 16 0
Step 6: Python Programming
MRAA has bindings for C and Python programming languages. Here is a simple example to blink the LED using the test circuit above with Python.
Use your favourite editor to add the following Python code and save the file as blink.py:
import mraa
import time
pin = 16 # set pin num
try:
gpio = mraa.Gpio(pin)
gpio.dir(mraa.DIR_OUT) # set mode as input
while True:
gpio.write(1)
time.sleep(1)
gpio.write(0)
time.sleep(1)
except KeyboardInterrupt:
print("\nstop\n")
Open a Terminal in the same directory as blink.py and run the following command to blink the LED:
python ./blink.py
Use CTRL + C to stop the program
Step 7: Next Steps
MRAA can be programmed with C if you need the best performance, but it is more complicated than with Python.
Other electrical interfaces can also be controlled with MRAA such as I2C, SPI, PWM and UART. Simple examples are listed on the Radxa website: https://docs.radxa.com/en/compute-module/cm5/radxa-os/app-dev/mraa
Further information can be found in the Eclipse Project website and Github repository:
- Eclipse MRAA https://projects.eclipse.org/projects/iot.mraa
- The MIT License (MIT) https://projects.eclipse.org/license/mit-license-mit
- MRAA Github https://github.com/eclipse/mraa
Summary
MRAA aims to be a platform independent way to access and control the GPIO on SBC’s. The Open Source project is run by the Eclipse Foundation so has wide industry support including upstream contributions from Radxa for the ROCK boards.
Hopefully, we have demonstrated how easy it is to start using MRAA in your ROCK projects to control hardware from the GPIO.
Comments