How do you feel about this article? Help us to provide better content for you.

Thank you! Your feedback has been received.

There was a problem submitting your feedback, please try again later.

What do you think of this article?
This includes the basic factors to consider when choosing an LED lens or reflector for your application. There is also information behind these factors to help you to make your decision.
A full PDF copy of the guide can be found at the bottom of the article.
Before you start…
Have you chosen your LED(s)? We offer a wide variety of LED products to choose from including standard LEDs and LED arrays:
Visible LEDs
COB LEDs
LED Arrays
LED Light Engines
WHAT ARE LED OPTICS?
LED lighting fixtures utilise at least one type of secondary optic to alter the beam of light coming from the LED source. At RS Components we have three families for secondary LED optics: Lenses, Reflectors and Optic & Holder Kits. Here is what you can expect to find in each family:
LENSES
LED lenses come in various shapes and sizes, for example round, square and hexagonal. Common lens materials include plastic and silicone. Therefore some are rigid and some are flexible.
Lenses are designed for use with single or multiple LEDs. This includes LED modules or strips.
They sit over the LEDs to create the desired lighting effect. Various properties of LED lenses enable precise control over the beams of light. LED lenses can also offer a nice aesthetic appearance by masking the LED components within.
REFLECTORS
LED reflectors sit over the LED to alter the beam of light. They are an affordable and easy-to-use solution for your lighting fitment. However, they do not offer as much control as LED lenses.
Reflectors are made using plastic and can be metal coated.LED reflectors are smooth or multifaceted inside and come in various different shapes. This enables them to create a range of lighting effects.
Some reflectors contain a sub-lens, for additional diffusion or control of the light.
OPTIC & HOLDER KITS
LED optic and holder kits contain both the LED reflector/lens plus a holder. These are called lens assemblies or reflector kits.
Lens holders provide a mechanical cut-off shield and can also be used to enhance performance. They are also much easier to install than a stand-alone lens.
Alternatively these kits may include an LED holder which holds the LED in place. The lens/reflector then simply twists on top.
FACTORS TO CONSIDER
Beam Angle
This describes the angle over which the light is distributed. Lenses and reflectors can be used to help create your desired beam angle.
Narrow beam angles, for example 40°, have a tight beam of light and are ideal for spotlights. Wide beam angles around 120° have a larger coverage for wide area lighting.
Clear/Diffused
Clear lenses provide a crisp-edged beam of light. A diffused lens has a softer edge. Diffusion can also offer a more uniform light output when multiple LEDs are used.
Number of LEDs per Lens
This refers to the number of LEDs that the lens is designed for. They can be for single LEDs or arrays of LEDs. Multiple LED lenses are ideal for wide area lighting, for example street lighting.
Lenses are often designed for use with specific LEDs. Check the manufacturer data for compatible LED options.
Some manufacturers pre-mount LEDs onto a board ready for the lens/reflector to sit over, saving you having to solder and line the LEDs up accurately.
Fixing Method
How will you attach your lens/reflector? Some optics come supplied with an adhesive tape backing ready to be stuck down. Other optics will simply twist or snap onto an LED holder. Some may need attaching with screws or specific clips from the manufacturer. Alternatively a glue is used to attach the optic. Please note that certain glues are not compatible, check the manufacturer data for more information.
Adhesive Tape
Lens/Reflector Material
Material | Description |
PMMA | Clear plastic, sometimes known as acrylic. PMMA is a cost-effective material which is common in lenses. |
PC (Polycarbonate) | Temperature and impact resistant plastic. It also offers great optical characteristics. |
Silicone | Lenses made of silicone are flexible. They are also resistant to effects of UV light. |
HRPC | Hyper Reflective PC is used in reflectors and is often white. It has strong reflective qualities. |
Aluminium Coated | Common in reflectors, aluminium gives a silver finish and helps with reflection of the light. |