Skip to main content

How to Build a Robot with an Arduino and 8051 Microcontroller

by arain786

When I first started to build my own robot, the most important step was understanding the purpose behind it—mainly to decrease human effort or manpower in simple tasks. This article is here to walk you through what I’ve used in my own projects, from the Arduino module to the 8051 microcontroller. We’ll go over explaining each of the components, like the ultrasonic sensor for obstacle avoidance, the DC motor, motor driver, and the robot body, all of which are required to make it work. These applications are not only exciting but are reshaping the world of electronics through compact IC designs that power everyday robots.

How to Build a Robot?

Robot Body

When building a robot, I prefer a plastic body with wheels on both sides for balance. The ultrasonic sensor is arranged at the front to detect any obstacle and trigger avoidance by making the robot move aside. If an object is detected while it's moving, the robot will continue to move safely, as shown in the image.

DC Motor

In my robot projects, I’ve placed two DC motors in the robot body, each rated at 6V, making a total of 12V. A DC motor is an electric motor that runs on direct current electricity, and it works using electromagnetism. The internal configuration creates motion when current flows through a conductor inside a magnetic field. This interaction causes a force that is proportional to the current. The external magnets with opposite polarity—north and south—create attraction, while the same poles repel, affecting how the robot is moved, as shown in the image.

Arduino Module

The Arduino module is an important part of the robot design, especially when using an obstacle avoidance kit. I’ve connected the 1st, 2nd, and 3rd pins of the Arduino to the DC motor driver and ultrasonic sensor. A receiver at the second pin helps detect objects, while common components like a capacitor, diode, battery, and power supply ensure stable operation, as seen in the image.

Motor Driver IC

To run the DC motor, I used a motor driver IC where specific pins like 3, 6, 11, and 14 are connected to it, while pins 4, 5, 12, and 13 go to ground. The input pins 1 and 2 link to the Arduino module, and the enable pin connects to the transmitter for proper control.

Ultrasonic Sensor

The ultrasonic sensor helps the robot detect any obstacles and sends a signal to the Arduino board or 8051 microcontroller. Based on the input, the command is sent to motor drivers to move the vehicle on an alternate path. I tested this on a metallic surface like a refrigerator body, and it worked well with DC motors, RF transmitter, receiver, and other components shown in the image.

Metal Detector

The metal detector works on the principle of electromagnetic induction and is often used in electronic projects. It has a coil or multiple metal coils that help detect metals buried in the ground. I’ve connected it to the robot body using a PCB, as shown in the image.

Push Buttons

The push button is made of plastic or metal, often from hard materials, and is used to reset the microcontroller or restart the program, as seen in the image of typical buttons.

8051 Microcontroller

The 8051 microcontroller from the 8051 series has 40 pins, including pins 4, 5, 15, 16, 18, and 19, which are connected to an encoder IC like the HT12E and push buttons on pins 2, 7, 8, and 9. A crystal oscillator, resistor, capacitor, and Vcc from a 5V power supply are added for stable operation. All components are fixed by connecting them to a printed circuit board, as shown in the image.

Conclusion

Building a robot with an Arduino and an 8051 microcontroller combines both creativity and core electronics knowledge. From integrating sensors for obstacle detection to using motor drivers, push buttons, and metal detectors, each component plays a vital role in automation. This hands-on project enhances practical understanding of microcontrollers, circuits, and real-world robotic applications, making it an ideal learning experience for students and enthusiasts alike.

I’m an Electrical Engineer with a strong passion for technology and innovation, specializing in circuit design, embedded systems, and automation. Alongside my engineering background, I’m also a skilled Content Writer, creating clear and engaging technical content, tutorials, and documentation that bridge the gap between complex engineering concepts and practical understanding.
DesignSpark Logo

Enjoying DesignSpark?

Create an account to unlock powerful PCB and 3D Mechanical design software, collaborate in our forums, and download over a million free 3D models, schematics, and footprints.
Create an account

Already a DesignSpark member? Log In

Comments