DesignSpark Circuit Simulator Maintenance on 23rd May at 15:00 UTC for 2 hours

Skip to main content
Sponsored by: RS Components

Sponsored by: RS Components

How to add NVMe SSD storage to Radxa ROCK Single Board Computers

by milnepe

In this project we show you how you can add NVMe SSDs using the ROCK’s M.2 adapters, providing dedicated, high-capacity storage (up to 2TB) with PCIe interface speeds 10 - 20 times faster than microSD cards!

One of the big advantages of the ROCK range is the ability to attach NVMe solid state drives (SSD) using the M.2 adapter fitted to most boards. This provides dedicated and durable large capacity storage (up to 2TB) with high speed capability, using the PCIe interface. Read / write speeds can be greater than 10x faster than SD or eMMC storage with a lifespan of several years, depending on usage.

If you are using your ROCK as a power efficient desktop system, or for image editing, program compilation or database storage, then an NVMe SSD storage solution will give improved performance and data security.

The root filesystem (rootfs) can easily and safely be mounted on the SSD using standard Linux tools whilst the system still boots from the SD card or eMMC storage. This avoids having to solder NAND chips or configure those where present, which requires specialist software and can stop your board from booting if used incorrectly.

Below is a summary of the M.2 support for NVMe SSDs on the current ROCK range:

ROCK PCIe Gen Lanes M.2 Key SSD Form Factor
ROCK 3A PCIe 3.0 x2 M Key M.2 Extension Board 2230 / 2242 / 2260 / 2280
ROCK 3B PCIe 3.0 x2 M Key 2280 underside
ROCK 3C PCIe 2.0 x1 M Key 2230 topside
ROCK 4SE PCIe 2.1 x4 M Key M.2 Extension Board 2230 / 2242 / 2260 / 2280
ROCK 4C+     Not Fitted  
ROCK 5A PCIe 2.0 x2 E Key M.2 E Key-to-SATA
ROCK 5B PCIe 3.0 x4 M Key 2280 underside

We tested using the latest Debian Bullseye CLI distribution with a Transcend MTE352T 128GB, M.2 2230 PCIe Gen3 x2 SSD (256-4684) on the ROCK 3A (256-3911) and ROCK 4SE (220-9536) .

For the ROCK 5B (249-3159) we used the latest Debian Bullseye KDE distribution and a Transcend MTE110S M.2 2280 128 GB PCIe Gen3 x4 SSD (187-1666)

The latest official Operating Systems for ROCK boards are available from the Software and Downloads Hub.

SSD performance depends on several factors including the capability of the ROCK board, the specification of the SSD and the OS, application software, and device drivers.

Difficulty: Intermediate Time: 1.5 Hrs Steps: 9 Credits: None License: None
Part Description RS Stock Number
ROCK 3A ROCK 3 Model A (4GB) Single Board Computer (256-3911)
ROCK 4SE ROCK 4 Model SE 4GB Single Board Computer (220-9536)
ROCK 5B ROCK 5 Model B 8 GB Single Board Computer (249-3159)
QC Power Supply 36 W PD + QC Multihead PSU Plug In Power Supply 5→20V dc Output, 1.75→3A Output (243-6356)
USB-C Cable Deltaco USB 2.0 Cable USB C to USB C Cable, 2m (276-7734)
SD Card Sandisk 32 GB MicroSDHC Micro SD Card (283-6581)
M.2 Extension Board M.2 Extension Board V1.6 for ROCK 4 Model C+, ROCK 4 Model SE (256-4998)
2230 NVME SSD Transcend MTE352T M.2 2230 128 GB Internal Hard Drive (256-4684)
2280 NVME SSD Transcend MTE110S M.2 128 GB Internal SSD Hard Drive (187-1666)
USB-to-Serial cable FTDI Chip 1m USB to UART Cable in Black (767-6200)
PC Linux / Windows / Mac Host computer  
Internet / Router Internet connection  

Step 1: Hardware

All of the ROCK boards support NVMe SSD storage using M.2 connectors, with the exception of the ROCK 4C+ which doesn’t have one fitted. Depending on the board you are using there are various options for fitting an NVMe SSD drive and form factors which are supported.

ROCK 3B, ROCK 3C and ROCK 5B
Both boards have M.2 M-key connectors and mounting bosses on the PCB, so support the SSD directly. The ROCK 3C mounts 2230 format drives on the top side and the ROCK 3B and ROCK 5B support 2280 format drives on the bottom of the boards.

2230 format SSDs are 22mm in width and 30mm in length. 2280 format drives are 22mm wide and 80mm long.

ROCK 3C and 5B - 2230 Format

ROCK 3A and ROCK 4SE
Both boards have M.2 M-key connectors on the bottom side so they require the M.2 Extension Board (256-4998) which mounts the SSD above the ROCK.

The Extension Board supports the following SSD formats 2230 / 2242 / 2260 / 2280 and all the parts required to install the SSSD (Not Included) are supplied in the kit.

ROCK 3A and ROCK 4SE

The image below shows the ROCK 3A we are testing, along with the extension kit, SD card, 2280 SSD and USB-to-serial adaptor.

ROCK 3A with Extension Kit

To assemble the kit, first of all connect the IPEX cable to the SSD adapter board and the IPEX to M.2 adapter.

For long format SSDs as a precaution put a strip of insulation tape over the unused screw holes on the adapter board to prevent any possible short circuits.

Insert the SSD into the M.2 M key slot on the adapter board. This fits in at an angle and is held down in place by the screw provided.

Warning: DO NOT overtighten the retaining screw or you will shear off the boss

Step 2: Flash SD Card

Before configuring the SSD an up-to-date operating system that boots from SD /eMMC storage is required. You can use the Getting Started guides for your ROCK board. Here’s the link for the ROCK 3A that we are using in this demo: https://www.rs-online.com/designspark/get-started-with-radxa-rock-3a-on-debian

Step 3: Serial Console (Optional)

Although this is optional, we recommend attaching a USB-to-serial cable to the GPIO header so that you will be able to view the serial console output as the system boots. It is also possible to login via the console if anything is not working as expected.

Connect the cable to the ROCK board as follows:

  • Black -> Pin 6, Yellow -> Pin 8, Orange -> Pin 10
  • Connect the USB-A connector to your PC.
  • Open a serial terminal application on the host PC. We use minicom on Linux or Putty on Windows
$ minicom -D /dev/ttyUSB0 -b 1500000

Note: the default baud rate for ROCK boards is 1500000 baud

USB lead connected for Serial Console

Step 4: Partition Table

Warning: All the following commands are executed as root so be careful to refer to the correct device when running them.

It is important to correctly identify the storage devices attached to the system. lsblk is the Linux utility that lists all the block devices (disks) and partitions (part) recognised by the system. Each disk can contain none or several partitions.

Login to your ROCK via the desktop or SSH in and in a Terminal session list the devices attached:

lsblk

The screenshot below shows all the devices on the ROCK 3A with NVMe SSD attached:

  • SPI Flash chip mtdblock0 (16MB)
  • SD card - disk mmcblk1 (29.7GB) with 3 partitions:
  • mmcblk1p1 (16MB) is mounted on /config containing configuration used as part of the boot stage.
  • mmcblk1p2 (300MB) is unmounted
  • mmcblk1p3 (29.4MB) mounted on / containing the root filesystem
  • zram0 (991.8MB) is a swap disk
  • nvme0n1 (119.2GB) is unmounted - this is the SSD that we will be configuring

Note: Not all ROCK boards will have the same block devices

Partition Table

Now change to root to gain sufficient privileges to be able to setup the disk. This is indicated by the prompt changing to the #.

The current state of the disk can be shown with fdisk, the Linux disk formatting utility.

sudo -s
fdisk /dev/nvme0n1

This shows that the drive needs a partition table creating before we can proceed:

Note: Use m to see all the commands available in fdisk

current state shown with fdisk

Create a GPT partition table:

Enter option g to create a GPT partition then w to write the partition table to the device.

Create a GPT partition table

Step 5: Partitioning

Now that there is a partition table, a new Linux partition can be created on the disk.

Use fdisk again but this time with the n option for a new partition and press Enter to accept the defaults, then w to write them to the disk:

fdisk /dev/nvme0n1

Partition using fdisk

Now if you run lsblk again you can see the new partition nvme0np1:

# lsblk

run lsblk to see the new partition

Step 6: Copying

To copy the rootfs filesystem from the SD / eMMC media to the SSD we need to discover the partition UUID for the rootfs on the SD / eMMC storage. This is mounted on the SD card device mmcblk1p3 in this example.

blkid is the Linux utility that displays partition UUID information for block devices:

blkid /dev/mmcblk1p3

The rootfs PARTUUID for this example is "22d9259d-1fae-427d-a08f-cde77ae4bf3b". Your ID may be different!

copy the rootfs filesystem

dd is the Linux utility for copying raw bytes.

Use dd to copy the rootfs - this will take a few minutes (10 mins for this SSD) with just a blinking cursor, so be patient and wait until the command prompt returns:

dd if=/dev/disk/by-partuuid/22d9259d-1fae-427d-a08f-cde77ae4bf3b  \
of=/dev/nvme0n1p1 bs=4M conv=sync,noerror 

Warning: dd will override the data on your drive so be careful to write to the correct disk / partition - you can read about all the options with: man dd

dd will override the data on your drive

Step 7: Resize

After copying the partition the SSD partition must be resized to use the full storage.

Resize the partition, fixing any issues with the following command:

resize2fs /dev/nvme0n1p1

Tip: Look out for warnings of issues, if there are any run the commands that are shown before re-running resize2fs again

Resize

Step 8: Mount NVMe

The penultimate step is to configure the boot process to mount the rootfs from the NVMe disk rather than the SD / eMMC storage.

Make a copy of extlinux.conf in case you want to revert:

cp /boot/extlinux/extlinux.conf /boot/extlinux/extlinux.conf.orig

Edit /boot/extlinux/extlinux.conf using vi or nano:

vi /boot/extlinux/extlinux.conf

Change the first entry for the rootfs which will be something like this:

root=UUID=22d9259d-1fae-427d-a08f-cde77ae4bf3b

to the NVMe partition

root=/dev/nvme0n1p1

Now reboot and the rootfs (/) should now be mounted on nvme0n1p1:

reboot

The board still uses the first partition on the SD card to start the boot process but now the rootfs is mounted on the NVMe drive.

rootfs is mounted on the NVMe drive

Step 9: Speedtest

Now you can run a speed test on your SD card and the NVMe SSD and see the difference:

lsblk
sudo hdparm -t --direct /dev/mmcblk1
sudo hdparm -t --direct /dev/nvme0n1

You should now have a really fast NVMe SSD setup (18x faster than SD)!!!

Speedtest

Troubleshooting

You may have to install fdisk and util-linux packages:

sudo apt install fdisk util-linux

If things don’t go to plan and you need to revert the changes to the SD / eMMC so the system boots again, you can remove the SD / eMMC storage and attach it to a USB reader on a Linux host.

If you saved the extlinux.conf file, mount the drive and then copy the original back:

mkdir -p /mnt/sd
sudo mount /dev/sda /mnt/sd
sudo cp /mnt/sd/boot/extlinux/extlinux.conf.orig /mnt/sd/boot/extlinux/extlinux.conf
sudo umount /mnt/sd

Then put the media back in the ROCK and it should boot and run from the SD / eMMC storage again.

You can check that the filesystem is expanded using df:

df -h /dev/nvme0n1p1

If the full capacity of the drive is not reported, run the resize command again.

If you need to reset your SSD back to its factory settings you can do this by installing nvme-cli:

sudo -s
apt install nvme-cli

List drives:

nvme list
Node       SN          Model                  Namespace Usage           Format      FW Rev 
---------------- -------------------- ---------------------------------------- --------- -------------------------- ---------------- --------
/dev/nvme0n1   H651350013      TS128GMTE352T-OKD            1     128.04 GB / 128.04 GB  512  B + 0 B  T0417A3 


Verify factory format:

nvme id-ns /dev/nvme0n1 -H
...
nsattr	: 0
nvmsetid: 0
anagrpid: 0
endgid : 0
nguid  : 00000000000000000000000000000000
eui64  : 0000000000000000
LBA Format 0 : Metadata Size: 0  bytes - Data Size: 512 bytes - Relative Performance: 0 Best (in use)

Secure format LBA 0 - use this format as above (default)

nvme format /dev/nvme0n1 -s 1

Now the drive is reset to its factory state, ready to be used again.

I'm an engineer and Linux advocate with probably more SBCs than a Odysseus moon lander
DesignSpark Logo

Enjoying DesignSpark?

Create an account to unlock powerful PCB and 3D Mechanical design software, collaborate in our forums, and download over a million free 3D models, schematics, and footprints.
Create an account

Already a DesignSpark member? Log In

Comments