Skip to main content

How Panasonic Enables the Future of Factory Robotics

by GreigRS
1

Panasonic Components Driving Next‑Gen Factory Automation

Robotics

As global manufacturing accelerates toward deeper automation, one truth is becoming increasingly clear: the future of robotics will be defined not only by advanced AI or precision mechanics, but by the reliability of the components hidden inside every actuator, controller and robotic joint.

Across the industry, Panasonic is championing this message, because they see firsthand how the smallest components often carry the greatest responsibility. And as robot deployments surge past 4.28 million units worldwide, the demands placed on these electronics have never been higher.

In this article, we explore why Panasonic believes passive components are foundational to the next era of robotic performance and how their technologies are engineered specifically to meet the real‑world challenges robots face every day.

Rethinking the Foundations of Reliability in a New Era of Robotics

Modern robots work in environments that would test even the most advanced electronic systems: high ambient temperatures, dense integration, relentless vibration and continuous 24/7 operation. As manufacturers push for lighter, faster and more compact designs, the expectations placed on internal power electronics grow exponentially.

Panasonic has long warned that miniaturisation without durability leads to systems that perform well on paper, but ultimately fail prematurely on the factory floor. That is why the Panasonic engineering philosophy focuses simultaneously on performance, endurance and environmental resilience.

Think of it this way, robots can only be trusted with increasingly critical tasks if the components inside them can be trusted to perform.

Capacitors: The Cornerstone of Stable Power in Harsh Conditions

Capacitors are responsible for smoothing power delivery, absorbing noise and stabilising circuits under load. But traditional ceramic capacitors (MLCCs), while compact, exhibit drastic drops in capacitance under high temperature or DC bias. In some operating scenarios, they can lose up to 80% of their effective capacity.

This is why Panasonic has taken a leadership role in promoting conductive polymer capacitors as a more robust, reliable alternative.

Why Panasonic’s polymer capacitors are redefining robotic power design:

  • Stable performance under temperature and load. Polymer capacitors preserve capacitance even under heavy DC bias, making them ideal for robotic joints and compact controllers.
  • Reduced component count. Where 10 or more MLCCs may be needed to stabilise a circuit, one polymer capacitor can often achieve the same result, saving space, weight and assembly time.
  • Enhanced vibration resistance. Panasonics hybrid aluminium electrolytic capacitors can withstand up to 30G of vibration without additional adhesive reinforcement, simplifying production processes.

And for robotic manufacturers, this shift is transformative. Fewer components mean more compact designs. Greater stability means longer service intervals. And vibration resistance means performance that doesn't degrade in demanding applications.

Engineering for Heat: Components That Withstand the Toughest Environments

High‑temperature operation is one of the defining challenges in industrial robotics. Inside a robotic arm, internal spaces can routinely exceed 100°C. Panasonic has invested heavily in capacitors engineered specifically for this reality:

Together, these technologies enable robots to operate continuously, even in thermal environments that would compromise standard components.

Inductors and Resistors: Unseen Components With Outsized Impact

While capacitors often receive the most attention, inductors and resistors are equally critical to robotic performance.

Metal‑Composite Inductors:

Panasonic’s MC inductors maintain stable inductance even at 150°C and resist magnetic saturation far more effectively than ferrite types. This ensures consistent power delivery in servo drives, switching regulators and high‑current applications.

Low‑Resistance Current Detection Resistors:

By significantly lowering resistance values, Panasonic resistors can reduce component surface temperatures by 30°C or more, improving efficiency and reliability across the entire power control system.

Anti‑Sulphur Resistors for Harsh Industrial Environments:

In manufacturing regions where sulphur exposure is common, standard resistors degrade rapidly. Panasonic’s anti‑sulphur resistors, using gold or high‑palladium electrodes maintains stability for thousands of hours where conventional components would fail.

These innovations underscore a key Panasonic belief that every component matters. A robot is only as reliable as the smallest part on its circuit board.

For The Robotics Industry Reliability Is Key

As automation expands into more sectors, manufacturers face an increasing pressure to deliver robots that are faster, lighter and more energy‑efficient. But these innovations should never come at the cost of reliability.

Panasonic’s position is simple: Sustainable innovation must be built on components that endure real‑world conditions, not just laboratory benchmarks.

Panasonic is committed to advancing the passive components that enable breakthroughs in robotics, and to working closely with manufacturers who share our belief in engineering for the long term.

Panasonic A Hidden Strength Behind Robotics.

The future of robotics will not be determined solely by algorithms or mechanical design. It will be shaped by the durability, efficiency and integrity of the components that keep robots moving, sensing and responding day after day.

Panasonic continue to lead in this space, pushing the boundaries of passive component technology and enabling robotic systems that are not only more powerful, but more resilient, more compact and more dependable.

Because when robots take on the world’s toughest jobs, they deserve components engineered to meet the challenge head‑on.

RS stocks a wide range from Panasonic, use the quick links below.

Panasonic Capacitors

Panasonic Resistors

Panasonic Inductors

Favourite things are Family, Music and Judo. Also, I have the ability to retain and quote useless facts, something that pleases me but can annoy others. My engineering hero - Isambard Kingdom Brunel
DesignSpark Logo

Enjoying DesignSpark?

Create an account to unlock powerful PCB and 3D Mechanical design software, collaborate in our forums, and download over a million free 3D models, schematics, and footprints.
Create an account

Already a DesignSpark member? Log In

Comments