Skip to main content

How do I use the Mirror tool in DesignSpark Mechanical?

This tutorial requires:

DesignSpark Mechanical V6.0

This is a premium feature available to DSM users on the Creator or Engineer subscription plans.

The Mirror tool allows you to create a copy (mirror copy) of any selected object. For example, you design one half of the frame of a pair of spectacles and use the mirror tool to generate the other half. This ensure your design is mirror symmetrical like the real-world object, and not just a plain copy.

Here is a demo clip:

Use the Mirror tool mceclip0_dd4713cc58bfe82775bdccb72508a9862c4e2b30.png in the Insert ribbon group on the Design tab to mirror any geometry that can be moved with the Move tool. Here are the key working principles:

  • You can insert a mirror plane between two faces, associating the faces so you can edit them together. You can copy a solid, surface, face, or curve from one side of a mirror plane to the other.

  • You can mirror curves, points, and axes without leaving sketch mode or cross section mode. When you mirror a curve, changing its geometry does not propagate to the other side.

  • You can mirror solids that contain patterns of features on a face, and the pattern will be updated on both sides. The pattern must be created before the solid is mirrored.

  • The plane becomes a persistent mirror once you create geometry using the mirror. The mirror relationship is maintained when you use other 2D and 3D tools to edit your design.

  • Mirrored components have a mirrored icon in the structure tree and maintain their mirror relationships when they are exported.

  • Mirrored objects are created on the same layer as the original object. Mirrored points do not maintain their mirror relationship.

Mirroring an object

1. (Optional) Create the plane you want to use as a mirror using the Insert Plane tool and position it with the Move tool.

2. Click Mirror mceclip0_dd4713cc58bfe82775bdccb72508a9862c4e2b30.png in the Create group. The Select Mirror Plane tool guide is enabled.

mceclip1_907dbc4ea4a5b580d1d1cf3497611a28d9a0dd01

3. Click the plane to use as a mirror. If you didn’t create a plane previously, simply click on the face of the side of the object where the mirroring should take place.

mceclip2_af5621d2f19a71b0d546e57811bb3f13a647a7c5.png

4. Click the Mirror Body or Mirror Face tool guide.

5. Mouse over the solids or faces in your design to preview the solid, surface, or face that will be created on the other side of the selected mirror plane.

6. Turn off ‘merge mirrored objects’ in the tool options, in case the mirror plane sits on the object’s surface and you don’t want the mirror copy to combine with it into 1 solid.

mceclip3_d0f9c0c5e4e2083887a4480a4739c1e5a9638bca

7. Now, click the object you want to mirror.

mceclip4_f1742c269e4c06d95295a6a23c20be6895282459.png

8. The mirror plane is created and will persist in other tools. You can click objects in your design or click a component in the Structure tree.

If you enclose a volume by mirroring faces, a solid is created.

Removing a Mirror Face or Plane

1. Click Mirror mceclip0_dd4713cc58bfe82775bdccb72508a9862c4e2b30.png in the Create group. The Select Mirror Plane tool guide is enabled.

2. Click the Remove Mirror mceclip1_b94851f3b0fc4adfa98bee19485e69736ef65339.png tool guide.

3. Click the face from which you want to remove the mirror relationship. You can also Box-select any number of faces.

mceclip2_27d4a53d68cf133b8e5df4ba23794762c3520c5e.png

You can now independently change this face without affecting the mirror relationship of the other faces on this object.

You can temporarily disable a plane in any tool. Select a mirrored face to display the mirror plane, then click the mirror icon to disable the mirror. Click the mirror icon again to enable the mirror.

Mirror Tool Options

  • Merge mirrored objects: When you use a face as the mirror plane, or when the mirror plane lies on a face of the source object, the two mirrored objects will be merged. Deselect this option to make a new object, as shown below.

mceclip0_f431a67bb6f0c7a10b0e7e7bc15ac952eaf2f922

  • Create mirror relationships: If you deselect this option, only the geometry is created and not the mirror relationship. Changes to either object will not be reflected in the other, as shown below.

mceclip1_140e7dc7e5230b9752b65160487caaaf62db1e3b

You can create a mirror plane between two symmetrical faces in your design.

Setting Up a Mirror Relationship

1. Click the Mirror tool mceclip0_9fd10c692e4a91c249832e7cdf00a672d7af70b7.png in the Create ribbon group.

2. Click the Setup Mirror mceclip1_ba63aaccc06a066aef677d284e61653a4bfcd661.png tool guide.

3. As you mouse over the faces in your design, the eligible faces are highlighted. A face is eligible if it is symmetrical to another face in your design.

4. Click a face.

5. Click a parallel face. The second face is highlighted in blue and the mirror plane appears halfway between the two faces. Edits to one face will now be mirrored on the other face. Geometry in between the two faces will be updated accordingly.

mceclip2_b2d8a6df0cfeda515bb2f623ad3059bd9d763e43.png

You can create mirror relationships by finding similar faces on the other side of an existing mirror.

Finding Similar Faces on the Other Side of a Mirror

1. Click the Setup Mirror mceclip0_2b94e25f0dfe6d854576975611b04dc0decd85da.png tool guide.

2. Click a face. Ctrl+click to select multiple faces.

3. Alt+click a mirror plane. Identical faces equidistant from the mirror plane are highlighted in blue, and a mirror relationship is created.

mceclip1_93306dd2f442a0c631e045842207c487c165423d.png

Mirror Tool Guides

The following tool guides help step you through the process. Use the Tab key to cycle through them. As soon as the tool guide switches, the cursor may change to reflect the active guide.

Mirror Plane

mceclip0_1a420d72a896c3deabdb3d3145cbb12a2e63dbf2.png

The Mirror Plane tool guide is active by default. Select a face or plane to use it as a mirror. (You can also use this tool guide to select another mirror plane to use if one is already selected.

Mirror Body

mceclip1_b506ceb24f6c10a6300d9f484e59ee2ad475ee45.png

The Mirror Body tool guide activates automatically once you select a mirror face or plane. Mouse over the solids in your design to preview the solid that will be created by the mirror. Click a solid to mirror it.

Mirror Face

mceclip2_70eb0d13f8821af172263c1027e5defa69df305e.png

Once you select a face or plane to use as a mirror, use the Mirror Face tool guide to select the faces you want to mirror. Mousing over the faces before you click them previews the face that will be created by the mirror. Click a face to mirror it.

Mirror Component

mceclip3_9bee4be47d4d17e9785de1d81dd6f7d6051cbded.png

The Mirror Component creates a left-hand transform and does not create a mirror relationship between the two components or subassemblies.

Setup Mirror

mceclip4_ba63aaccc06a066aef677d284e61653a4bfcd661.png

The Setup Mirror tool guide can be used any time to create a mirror plane between two faces. Only those two faces will be affected by the mirror. To create a relationship among many faces, Ctrl+select faces and then select a mirror plane to auto-detect identical faces equidistant from the mirror plane.

Remove Mirror

mceclip5_d4e15fb3f409d584272eb25cc098a9cdec41c8b1.png

Use the Remove Mirror tool to remove the mirror relationship between faces. You can select to faces with a mirror relationship or use box-selection to select any number of mirrored pairs.

Mirroring Examples

1. A mirrored solid with a pattern of features is updated when the count is changed from 7 to 5 on one side.

mceclip0_94bc0b8782c69168da876d9a206175789c086050.png

2. Mirroring a sketched circle. Modifying the circle does not change the geometry of the mirrored circle

mceclip1_73010aba33b5e2e469e269972da497c4957b5457.png

3. Mirror associations are maintained in the Pull tool using the Copy Edge and Extrude Edge options. The behaviour for Copy Edge is on the left and Extrude Edge is on the right.

mceclip2_be7daf967681133c5ed0b8f3478d639c9e20730b.png

4. A mirrored surface body that becomes a closed body after the mirror now becomes a closed body. Start with a solid body, detach a face to make two surface bodies, and create a plane at the opening.

mceclip3_6a897df8b0b30b6b4365ef0bf42570427d76d791

5. Mirror the surface body to see a solid body with the detached surface in the mirror plane.

mceclip4_d46b4ed85cd91d44446c945725c84711d11bad3f.png

RS DesignSpark is the go-to platform for students, makers, hobbyists and professional design engineers, providing design resources such as the award winning DesignSpark PCB and DesignSpark Mechanical CAD software. Join the community today at https://www.rs-online.com/designspark/register

Comments