DesignSpark PCB: New Version 13 - NOW AVAILABLE

Skip to main content

How do I place tracks on my PCB with different features?

by DesignSpark

This tutorial requires:

DesignSpark PCB V11.0.0

You have just completed your schematic; how do you place the copper tracks on the PCB and customise them to your design layout?

1. Here we have a simple example of a two-component schematic. Nets connect the pins of each connector in a simple one-to-one arrangement.

Component Schematic

2. We now wish to produce a PCB. 
From the menu bar select Tools --> Translate To PCB…

Select Translate to PCB

3. Use the PCB wizard to generate the required PCB size and layer requirements. 

Drag the components to their required positions and you will see as in the example the components connected by their ‘air wires’, commonly called a ‘rats nest’. These are not the copper tracks! It is now your task to route these in copper.

Air wires

 

4. From the tool bar select the “Add Track” icon. The pointer is now in a mode ready to place the copper.

Add Track

 

5. Click on the air wire to route, the track appears from the pad and you may route the copper as you wish completing the track.

Tips:
1. Do not click the pad as this will place copper but not remove the air wire.
2. You may right-click and see options such as changing the track width as you progress.

Click on air wire

 

6. The default is Orthogonal placed tracks. You can select other options from the ‘right click’ menu such as ‘miter’ which is a very common routing style. The options are illustrated below.

Segment mode

 

7. Should you wish to edit any part of the segment, (press ESC to exit the ‘Add Track’ mode) click on the required part (and CTRL + left click to select additional parts of the track) to highlight and press the short cut key combination CTRL + U to ‘undo’ the routing but retaining the air wire connectivity.
Remember the ‘undo’ icon will progressively undo track placement from your latest step which may be a useful fast editing method.

Tips:
1. DO NOT use the delete key as you will remove the air wire connectivity. Should you accidentally do this use ‘undo’ to recover the air wire.
2. When re-tracking the air wire part of the segment, use ‘Add Track’ as before and click on the air wire or attach the route to this.

undo and add track

 

Remember there is much more additional detail in ‘Help’ from the menu bar or by Shift + F1.

RS DesignSpark is the go-to platform for professional design engineers, providing application and product content and design resources such as the award winning DesignSpark PCB and DesignSpark Mechanical CAD software.
DesignSpark Logo

Enjoying DesignSpark?

Create an account to unlock powerful PCB and 3D Mechanical design software, collaborate in our forums, and download over a million free 3D models, schematics, and footprints.
Create an account

Already a DesignSpark member? Log In

Comments