Skip to main content

How do I make an image wrap around a 3D object?

by DesignSpark

This tutorial requires:

DesignSpark Mechanical V6.0

Wrap Around option is not visible until you are adding an image. Note that wrapping an image does not mean it will 3D print with your STL file. The image exists separate to your CAD model and is not part of the geometry yet. You can use various sketch tools (like, spline) to draw an outline of the image and then either:

a. Use the project tool to add it to a curved surface.

b. Convert to an independent surface, use Pull tool to get a solid and export it to STL (if you only want to 3D print a flat logo).

Here are the steps to simply wrap an image without adding to geometry:

  1. Make a sample 3D object like a cylinder

     

    blobid0_283430ad8ecaad9962539c17ddbe6f593ec6fa67.png

  2. With the cylinder in the Design View, you then select the File in the insert menu to pick your wrapping image.

     

    blobid1_c8ba34b03e20dad2ee61a480d071d380300714ed.png

  3. Then select the Logo. In this case, we use an RS logo have saved to Desktop.

     

    mceclip1_0b8a42428142003c757a6f5037f156e8fd9bfe8a.png

  4. After clicking open, the image will stick to your mouse pointer waiting to be placed. You then select the 'Place wrapped Image' option in the Design View, the other option is a flat surface placement option for image.

     

    mceclip0_54991a05c1ec4c9defddb0efade2648a51fd2d19.png

  5. Once the Wrap Around option is selected, you then select the surface of the Cylinder as this is where you want the wraparound. You can position before you set it and scale its size by using your mouse scroll wheel.

     

    Here is a screen shot of how the RS logo Image looks wrapped around.

    mceclip2_40801c94f9f436664c3057df6464b9d5c2a3fb97.png

RS DesignSpark is the go-to platform for students, makers, hobbyists and professional design engineers, providing design resources such as the award winning DesignSpark PCB and DesignSpark Mechanical CAD software. Join the community today at https://www.rs-online.com/designspark/register
DesignSpark Logo

Enjoying DesignSpark?

Create an account to unlock powerful PCB and 3D Mechanical design software, collaborate in our forums, and download over a million free 3D models, schematics, and footprints.
Create an account

Already a DesignSpark member? Log In

Comments