Skip to main content

How can I prepare part models for 3D view?

This tutorial requires:

DesignSpark PCB V11.0.0

The following is an exploration of the 3D View and how components are assigned their 3D representation. Here we have a simple 2-component example with components downloaded from PCB Parts Library.

2D View of components

The DIL component is automatically assigned a 3D image from the package name. Here the DIP762W70P is identified as having 'DIP' in the name by the Alias DIP assigned to the 3D component.

DIL component is automatically assigned a 3D image from the package name

The 3D View appears with the assigned 3D representation as shown.

3D View

The LED however does not match any 'package' entry so is represented by a block of the size of the component boundary, this is the rectangle that encloses the component hence the square shape.

We shall now look for a suitable 3D model for the LED. In the Library Manager on the 3D tab select 'All Libraries' and you will see a list of available 3D components (check you have the default installed libraries enabled on the Folders tab) which can be viewed to select the appropriate model, or use 'Find' to help locate one.

Here I have located a suitable component.

Selecting suitable component from library

To use this in the 3D view we need to add our package to the 'Alias' list, this is from the package assigned, which in this case is LED_5MM. To achieve this, with the 3D component selected click the 'Edit' button and a new window is launched. Here against the 'Also Applies' click 'Add' and enter the required component PCB Symbol package name. Click OK and close all the windows.

Add component to Alias list

Now when you launch the 3D View it will have the assigned model.

2D View with LED shape correctly displayed

If the component height is not correct this can be set in the 'Values' for the component as has been done above.

Edit the height of LED

Please see the embedded help file, coming with the DSPCB installation file, for further explanation of how to use 3D PCB view and how to prepare custom 3D view part models.

Help file

RS DesignSpark is the go-to platform for students, makers, hobbyists and professional design engineers, providing design resources such as the award winning DesignSpark PCB and DesignSpark Mechanical CAD software. Join the community today at https://www.rs-online.com/designspark/register

Comments