DesignSpark PCB: New Version 13 - NOW AVAILABLE

Skip to main content

How can I add a fiducial mark to my PCB?

by DesignSpark

This tutorial requires:

DesignSpark PCB V11.0.0

With an Engineer subscription, DesignSpark PCB has additional features which provide greater control and simplify the process to allow a fiducial library component to be produced.

For DSPCB users, before discussing the fiducial, the following tutorial is a technique to allow DSPCB users to create a fiducial. The process described is performed in the PCB editor, not the Component editor.

What is a fiducial mark?

Fiducial marks are used for position referencing by imaging systems when components are being placed.
They consist of a small, filled circle of copper and a clear area from the solder resist layer and usually a minimum of two are placed in diagonally opposite corners of the board. In some situations, with high-density areas of small surface mount components, additional fiducial marks are required local to that area.

There is not an official recommendation on the size, number or positioning of fiducial marks so it is recommended that you discuss with your manufacturer for their recommendations.

Various suggestions are made on the internet that the solid copper area should be 1 to 2mm diameter and the clearance in the solder mask twice this, e.g. 1.5mm diameter copper and a 3mm diameter clearance in the resist.

Pads cannot be used as they do not have the required control over solder mask and paste mask, however, it is quite simple to create the fiducial on your PCB layout as follows.

Creating a fiducial.

The use of the "Add Shape Circle" provides the required flexibility for this.

Add Shape Circle option

However, before adding the shape, assuming you wish to add a 1mm diameter copper area and a 3mm aperture in the solder mask it is easier if you set the grid to 1mm and snap to grid to half or quarter grid. This allows the easy location of the shape and snapping to a 1mm diameter.

Grids - Settings

Select the "Add Shape Circle" and right-click before placing and ensure "Filled Shape" is set, you may also select the Layer or change layers after placing as shown.

Select Add Shape Circle and Change Layer option

Place the circle shape and expand to the next half-grid line. Note grid setting in this example are 0.5mm.

Place circle shape and expand

If required then change the layer using the "L" key shortcut or select the object, right-click and select "Layers". Change the layer to Top Copper.

Change layer

Repeat for solder mask exclusion area by adding another closed circle shape over the copper shape and change the layer to Top Solder Mask. The solder mask is a negative image, the shape will correspond to the excluded area of solder resist.

Change layer for solder mask

The fiducial is now created, use F5 to redraw the view.

Fiducial is now created

At this point it is good practice to select the fiducial, right click and select 'Group', this will prevent the copper circle and solder mask from becoming misaligned.

Further fiducials can be simply placed by selecting the fiducial and copying by CTRL+C and pasting by CTRL+V.

Copying fiducials

Although the fiducial cannot be saved as a library component a quick and easy solution for future use is to save the fiducial as a PCB design with the fiducial. When working on a new design also open this PCB design and you can copy and paste the fiducial to your current design as shown below.

Save fiducial as a new PCB design

Sample file

The fiducials.pcb file contains various fiducials for you to examine and use as required and is attached.

NOTE. When you produce your plot files please ensure that "Pads-Only" is not selected or your "shapes" will not be included in the plots!

Output Manufacturing Plot options

RS DesignSpark is the go-to platform for professional design engineers, providing application and product content and design resources such as the award winning DesignSpark PCB and DesignSpark Mechanical CAD software.
DesignSpark Logo

Enjoying DesignSpark?

Create an account to unlock powerful PCB and 3D Mechanical design software, collaborate in our forums, and download over a million free 3D models, schematics, and footprints.
Create an account

Already a DesignSpark member? Log In

Comments