Skip to main content

How can I add a drawing border/template to the schematic design?

This tutorial requires:

DesignSpark PCB V11.0.0

DesignSpark supplies a number of schematic sheet templates for use in DSPCB.

These include A1, A2, A3 and A4 and ANSI A, B, C and D, and also "Letter" for you to use.

Note ANSI sizes are based on the inch paper size:

blobid0_eec0b6cd6526ec4448286048f5a3f2562cdce769.png

At any time, you can add a drawing border to the design.

Using the Add Component browser (<F9>), select the "schema" library from the drop-down list.

NOTE: If you do not find the schema library check that you have enabled the supplied Library.

https://www.rs-online.com/designspark/how-do-i-set-up-my-libraries

blobid1_893b9a122a055260fccc9ca6a46d5b2ca8ec2a96.png

For reference, this is a schematic only component library these symbols will not have any PCB symbols associated with them.

There are also many other useful schematic only symbols such as TO and FROM and voltage rails.

Scroll down the list and select the required drawing border that has been created to fit the appropriate paper size.

blobid2_3b65b315846b33f5ad0636893fa1e27558a89212.png

Just like other components, select say A4 from the list and click <Add>.

Position it as required. You may need to zoom out a bit to see it all to place it. Use the <Z> key to zoom out or <A> to view all of the design. For speed you can also roll the mouse wheel.

The form will appear as below:

blobid3_10b6b17fb96c939eb4a75135ad17195441fb87d2.png

All the text fields can be customised and you can save the customised template in your own library.

blobid4_27c0014398012bfaf38c8cb8e8cf2ff2bab611d5.png

RS DesignSpark is the go-to platform for students, makers, hobbyists and professional design engineers, providing design resources such as the award winning DesignSpark PCB and DesignSpark Mechanical CAD software. Join the community today at https://www.rs-online.com/designspark/register
DesignSpark Electrical Logolinkedin