Buiding images based on Debian or Ubuntu with 6.1 linux mainline and 5.15 is not building correctly. Sure I get the development environment to build linux operating systems built ok, including u-boot, but flashing bookworm, bullseye or buster to sdcard just creates:
DOS Partition Table
Offset Sector: 0
Units are in 512-byte sectors
Slot Start End Length Description
000: Meta 0000000000 0000000000 0000000001 Primary Table (#0)
001: ------- 0000000000 0000032767 0000032768 Unallocated
002: 000:000 0000032768 0002441215 0002408448 Linux (0x83)
Which obviously doesn't boot:
[Debug terminal output]
U-Boot TPL 2022.07 - armbian
rk3399_dmc_of_to_plat: Cannot read rockchip, sdrams-params -1
DRAM init failed -1
I am trying to get docker up and running as I want to use it in my project. I received a starter kit, put it together and it booted up ok from the sdcard. Updated and upgraded it, I installed docker and tested to find it wouldn't run as it required a vital net component, '...VLAN_BRIDGE...' to be installed, but it was missing in the kernel configuration. Followed the prompts to reconfigure the kernel (rebuild my own kernel) only for it all to come crashing down before my eyes a few hours later and before the build had finished.
Previously:
I downloaded ubuntu focal server for this ROCK 4C+ card expecting it to have the component installed ... it didn't, then debian bullseye kde version also missing the VLAN_BRIDGE component (I wasn't really expecting it to have it configured being a desktop version, but the server, I thought, yes!).
I have gone a bit further with my Armbian builds partition and dd'd idbloader.img and u-boot.itb onto the sdflashcard at the appropriate places, but it hasn't made any difference to the boot, and as far as I can tell there is no extlinux.conf on any of the armbian images. I probably should flash the boot.img, but all I can find is a u-boot.img, so I haven't tried it yet.
This is what my ubuntu focal server edition partition looks like:
GUID Partition Table (EFI)
Offset Sector: 0
Units are in 512-byte sectors
Slot Start End Length Description
000: Meta 0000000000 0000000000 0000000001 Safety Table
001: ------- 0000000000 0000000063 0000000064 Unallocated
002: Meta 0000000001 0000000001 0000000001 GPT Header
003: Meta 0000000002 0000000033 0000000032 Partition Table
004: 000 0000000064 0000008063 0000008000 loader1
005: ------- 0000008064 0000016383 0000008320 Unallocated
006: 001 0000016384 0000024575 0000008192 loader2
007: 002 0000024576 0000032767 0000008192 trust
008: 003 0000032768 0001081343 0001048576 boot
009: 004 0001081344 0062584927 0061503584 rootfs
010: ------- 0062584928 0062586879 0000001952 Unallocated
Next step might be to write some of this stuff into my armbian build partitions / spaces. Any one else in the same boat? I wonder why there is no support for docker in the downloadable images for the ROCK 4C+?
The article quoted at the beginning is old and you should use 6.3 edge and 6.1 current and yes, 6.1 has ROCK 4C+ support built in as stated in the article. Adding support in the Armbian build for ROCK 4C+ (rock-4cplus) and copying the defconfig before hand though works fine.
It's been a while since I installed linux, earliest I remember was RedHat Linux 5.2 which came bundled on a magazine as a disc back 30 years ago.
The ROCK 4C+ board doesn't have a SPI or the USB3.0 OTG option not a lot going for it! Or am I missing it?
Built images are not working, so what has to be done? All this, leaves my project way off in the background, right out on the Edge.
Sorry, if I haven't been much help, I am sure you can fix this though. And apologies if this post is in the wrong forum as my first thought was to post in the 'Getting Started Forum', still think so! :)