DESIGNSPARK FORUMS
Communicate freely with other DesignSpark members via the forums area. Create new conversations or join existing discussions about products, technology, software, and future innovation.
Help to provide solutions or seek answers to your own technical problems by calling upon a global network of like-minded engineers.
I didn't know drawing views were so adaptable...
Broken views and broken out sections can also be utilised to make Partial views..
'Local Detail view 'A' can have additional 'Projected view' added, which is then selected becoming the Aligned Sections host which an additional 'Broken' view has then be added. Then the unwanted 'Broken' view ( side or sides) can be deleted. Alternatively, if the broken line is outside of the model, then only 1 partial view is made.
Partial View of the scalloped angled face is actually a broken out section with the remaining scallop 'outside' of the broken section. The original projected view that the whole view ( latterly becoming a partial view) was projected from, then has had an subsequent 'Broken' view applied to it using a spline - breaking this view into two views with the unwanted view then being deleted.
All this is a bit of a long way around but it achieves exactly what is needed.
The scrap view under D-D is made from a broken out section.
The pivot tool for 'Aligned Sections' is just amazingly fast with such a simple and few click process.
The ziz zag broken lines seem to be non functional at the moment, I've reverted to spline breaks which I quite like now.
Above local sections and views etc were made with v6.0.3
Over the years many amazing projects have been created using DesignSparks tools and resources. New businesses have started their journey with DesignSpark, creating prototypes and taking their products to market. Others see DesignSpark as a key component within their engineering functions, adding value and providing the opportunity to design.
Today, DesignSpark offers you an engineering and design ecosystem where you can turn your ideas into reality.
Provide a DesignSpark testimonial so we can share with others.
Simply fill in the form on this page
https://www.rs-online.com/designspark/creator-your-own-testimonial
I have an assembly with multiple copies of parts. The parts I've designed from scratch all behave as I want, if I move one the other stay still, if I change the design of any part all get the same design change.
However I've some parts which where originally STP files I've converted to rsdocx. For these parts if I move one of them all the parts move the same (component or object selected). I can make them independant, but then I end up with multiple copies of essentially the same thing.
I made them docx as I may want to make changes and I want to link a drawing to the part.
How can I stop this happening and the converted stp files behave the same as scratch drawn parts ? Hi DS Mechanical users, we at DesignSpark have now upgraded the discussion forum
with a 'pin to top' feature.
This means that above the headline, you can see discussion threads from users that we think can be helpful to everyone using DS Mechanical.
If you scrolled past it, it's above the Create new post and looks like this:
What do you think of this new feature? Let us know in the comments below. Hi DS PCB users, we at DesignSpark have now upgraded the discussion forum with a 'pin to top' feature.
This means that above the headline, you can see discussion threads from users that we think can be helpful to everyone using DS PCB.
If you scrolled past it, it's above the Create new post and looks like this:
What do you think? Leave a message below in the comments.
I tried to add a panel meter to the library.
The PCB symbol includes a rectangular outline with rounded corners:-
I added a new entry in the 3D View library with Package Style set to 'Shape'. The preview looks as expected:-
However the resulting 3D View does not work - you only get a flat 2D outline:-
If I change the Package Style to 'Box' then it works (except there are no rounded corners of course):-
This has to be a bug.
Da wir von DesignSpark in letzter Zeit von Problemen mit dem Abschließen einer Mehrplatzlizenz hören, möchten wir erneut auf den Hilfe-Beitrag aufmerksam machen, den wir im Februar erstellt haben.
https://www.rs-online.com/designspark/how-to-request-a-quote-for-multiple-designspark-users-in-your-organisation-de
Alle weiteren FAQs zu Abonnements finden sich hier:
https://www.rs-online.com/designspark/subscriptions-support-faqs-de
Sie haben Fragen? Stellen Sie uns eine Frage hier in den Kommentaren oder wenden Sie sich an den Helpdesk.
Viele Grüße, Stephanie und das DesignSpark Team
製品のデータを描いたのですが、y軸とz軸を間違えたまま書いてしまいました。
出来上がったデータのy軸とz軸を入れ替えることは出来ますか?
よろしくお願いします。 v6からインストールできる台数が1台とありますが、PCを更新した場合はどのように、再(新規?)インストールすればよろしいでしょうか?
When I went to open DS, version 10 booted up without any issues, but version 11 indicates that there is an activation issue, meaning there is a communication issue between your server and the program during startup.
Since upgrade from v8 to v11, links to companent packages have been broken, still shows component and going into the preferences for it, still shows the package name.
When generating pcb it comes up with multple errors for component packages, how can this be fixed without having to redo companent libraries? Bonjour,
J'ai routé plusieur PCB, et afin de vérifier les laisons entre les connecteurs.
Est ce qu'il y a une méthode de valoir extraire un tableau de coordonné des nets pour vérifier avec qu'il a été demandé ?
par exemple: J2.C2 vers J1.A15 Guten Morgen zusammen,
ich benutze DSM jetzt seit einer Woche und finde es sehr intuitiv. Das Einzige, was mir aufgefallen ist, ist, dass bei der Zeichnungserstellung die Projektierungsmethode 3 verwendet wird und ich das nicht ändern kann (oder noch nicht gefunden habe). Das wird immer wieder zu Diskussionen mit alteingesessenen Fertigern führen ;-)
Gibt es eine Funktion dafür oder etwas beim erstellen der Zeichnung das mir nicht aufgefallen ist?
Google Translation:
Good morning everyone,
I've been using DSM for a week now and find it very intuitive. The only thing I noticed is that project planning method 3 is used when creating the drawing and I can't change that (or haven't found it yet). This will always lead to discussions with long-established manufacturers ;-)
Is there a function for this or something I didn't notice when creating the drawing? Bonjour,
Comment corriger ce probléme Drill Hole to Dril Hole ?
Merci d'avance
We know you’re interested in annual multi-set licenses for your team!
Join the club! Engineers just like you, are enjoying the perks of a multi-seat license:
1. Speed, convenience, and effortless set up. You can now manage Creator or Engineer subscriptions for your whole engineering team giving you the flexibility and control you need.
2. Improve collaboration within your team, with suppliers and business partners. Your whole team can now access 3 professional tools in one subscription that complement any toolbox.
3. Count the savings and give your budget some extra wiggle room with a year-round discount. Save between 5 – 10%, depending on the number of licenses your purchase.
Ready to make this happen? Complete the request a quote ticket to grab your exclusive discount, set up your preferred payment, and assign seats to your team members.
Get ready for a year packed with brilliant resources and benefits. We can’t wait to have you onboard.
Watch the video to find out more on how to request a multi seat license
https://youtu.be/BP7MUfDTTZg
New Posts
Drawing views - Auxiliary Partial ... use Projected and Broken custom views and transfer model dimensions
We'd like to hear from you! Create your DS testimonial
STP converted to rsdocx files are linked if multiple copies are in an assembly ?
Info for all DS Mechanical users
Info for all DS PCB users
3D View not working for some shapes
Sie haben Fragen zur Mehrplatzlizenz? Hier sind die Antworten
Y軸とZ軸の入れ替えは出来ますか?
PCを更新した場合のアカウントは?
Can't start DS
Lost Libraries
Extraire un tableau de nets
Projektionsmethode in der Zeichnungsableitung
ERROR (D-D)
Share DesignSpark with your team! How can you set up a multi seat license?
Our forums
Software
Activist Engineering
Building our Air Quality Kit
- posts
- 16