Skip to main content

Examples of Drawing BOM types


Within a drawing, Top Level, Indented or Part's Only BOM tables are available.

This is a quick description of the basic functionality of BOMS and how a BOM table can be modified.

Only components with an 'Add to BOM' right click command will be shown in the BOM table. Multiple components can be selected > Add to BOM.

mceclip0_3fd8c647bd18e69632ee70192b6a33c5498a4a2b.png

 

Example of  Top Level BOM:

Showing the 1st level of a structured design:

mceclip11_f43bf4289d34a58b52b3957eb9c46469e5093d03.png

mceclip1_c9fad7acf2c55f2d6acbe8c82a23a5cc98674d32.png

Example of Indented BOM:

mceclip0_68b92cfd386fe02e4c9a5997d8882ce3b5532c24.png

mceclip3_037e7f3c0f2e96511024354569ed5c318385d39b.png

 

Example of Parts Only BOM:

Assembly owning components are not described - only parts are listed

mceclip2_8feb0f77cdc63c1401b87dabf62375149162fa05.png

Notes on BOM Tables:

Within any BOM table, rows or columns can be sorted , added or deleted. The table can also be split:

Examples:

Parts only BOM table it's possible to re-order the ' ITEM NO.' by just selecting and changing the number,  then sort the column as shown below:

mceclip7_4a85aa9b4ba4caa1f96c40f61ebe5ddfeb534d69.png

 

 Also, by selection of any row item description such as Item no, Description, Quantity etc, it is possible to Insert a row which then allows to add spaces within the table ( spaces must retain a 'Item number'). All ballooned items automatically update their numbering. *See the example below showing items 7 and 8 as empty components:

* Having numerical gaps allows for the Insertion or deletion of items without affecting the Item number of other items which could be important it other documents reference the BOM table.

mceclip6_7e3777484835e5e5189ba39fa8ea8c262207956b.png

 

In the example below of a Indented BOM, the table has been Split into each assembly. This allows for each table to be repositioned close to their parts within the drawing:

Note: Do not add a row to an Indented BOM.

 

mceclip10_0fea7e44d64346c9d9dbf0cf19da57b82c5d7666.png

mceclip8_9c2d7ac186d61b58ca804abaa95ea6a03de7ef7d.png

 

 

 

Comments