I have some old stp assembly models from which I create sales drawings in DS, in the structure tree each "part" shows up as a solid rather than seperate component. When I create the drawings the text for Diameters is at the same angle as the primary leader, as below, diameter 8.0 and 60.1. If I create one of these solids as a "new" component in DS then for same dimension the leader is split and the text horizontal see lowest screenshot, which is how I want it and it usually appears.
.I have played with annotation planes and checked all the DS options but cannot find a way around this.
How can I make the dimension text horizontal ?
Comments