Development of Anaerobic Bio-Batteries from Banana Waste using Synthetic Microbial Pathway.
The rapid industrialization and population growth have made the provision of sustainable and reliable energy one of the most critical challenges for the future. As a result, there has been a shift towards developing improved batteries that offer enhanced energy storage densities, improved safety, fast rechargeability, biodegradability, and minimal environmental footprints.
A battery, by definition, stores chemical energy and converts it into electrical energy through electrochemical reactions, involving electron transfer between two electrodes: an anode (negatively charged) and a cathode (positively charged). Due to their compact size and portability, batteries are one of the most promising technologies for direct electrical energy storage. Storing electrical energy in batteries provides a viable solution to the challenges posed by the rapid expansion of renewable and variable energy sources on both small and large scales.
Bio-batteries present a sustainable alternative to traditional lithium-ion and lead-acid batteries. They have the potential to generate on-demand, cost-effective, portable power and are a non-toxic, non-flammable energy source. This research explores the development of rechargeable bio-batteries using anaerobic microbial pathways for the storage and generation of electrical power. In this process, bacteria metabolize organic matter, converting chemical energy into electrical energy. Bacteria-based bio-batteries represent an innovative approach to the valorization of organic waste for energy generation. Moreover, waste management policies underscore the importance of energy recovery from waste before its disposal.
Bananas, the second most produced fruit globally, play a crucial role in economic development and food security, especially in developing countries like those in Africa. However, the annual production of approximately 114 million metric tons of banana waste presents significant environmental challenges, such as nutrient leaching and methane emissions. Typically, banana waste is either dumped in landfills or repurposed as fertilizer or animal feed. To mitigate these environmental concerns, sustainable alternatives for valorizing banana waste are being explored. Notably, banana waste can be harnessed to generate electricity, making it a promising substrate for bio-batteries. The fruit peel contains energy-rich compounds like glucose and cellulose, which can be metabolized by exoelectrogens - microbes such as Geobacter and Shewanella Oneidensis - to produce energy through microbial metabolism.
While bio-batteries hold significant promise, further research is needed to optimize their performance. Determining the optimal ratio of bacteria to organic matter for improved energy density, thermal resistance, and charge-discharge cycling is crucial. This research aims to advance the understanding of anaerobic bio-batteries by evaluating the effects of varying bacteria and organic waste compositions on battery characteristics. The goal is to decrease the overall cost of batteries, making electrical energy more accessible in Africa. This is particularly important in Sub-Saharan Africa, where low access to modern energy, combined with high urbanization and population growth rates, is expected to exert increased pressure on existing energy infrastructures and government budgets, introducing uncertainty in the future path of resource consumption. Through this research, we aim to not only contribute to the field of sustainable energy but also to offer practical solutions that could transform waste management practices and energy accessibility in regions where it is needed most.
The primary objective is to optimize anaerobic bio-batteries for maximum power density, stability, and longevity, using banana waste as a substrate. The project targets three bacterial strains—Escherichia coli, Shewanella oneidensis, and Geobacter sulfurreducens—to determine which provides the highest energy output. The goal is to create a cost-effective, biodegradable battery that could significantly impact energy accessibility in Africa and contribute to global efforts towards a circular economy.
The project will utilize funding from RS to purchase materials and equipment necessary for the fabrication and testing of the bio-batteries. Please refer to Table 1 below for an overview of the materials and equipment to fabricate the battery and to characterize the batteries' performance. These resources are crucial for achieving the project's goals and ensuring the bio-batteries are both efficient and sustainable.
| Item | Price (Rand) |
|---|---|
| Consumables and reagents | 3,000.00 |
| Fabrication of biobattery module including the plates | 1,000.00 |
| Nafion membrane | 1,000.00 |
| Bacteria | 2,000.00 |
| SEM analysis | 1,000.00 |
| TGA analysis | 1,000.00 |
| Optical or Epifluorescence microscope | 1,000.00 |
| Total | 10 000.00 |
Table 1: List of materials and equipment required for the fabrication of bio-batteries
The next steps involve varying the bacterial ratios and substrate concentrations to achieve the desired power density and battery longevity. Challenges anticipated include managing the variability in bacterial growth and ensuring consistent battery performance. Success will be measured by the ability to generate a stable power output with a low environmental impact, potentially leading to real-world applications in areas with limited access to reliable energy.
Comments