Skip to main content

Comparing DesignSpark PCB and DesignSpark PCB Pro Interfaces

You might be wondering what the buzz around DesignSpark PCB Pro is. If you have been using DesignSpark PCB for a while and not sure whether it is worth switching to the professional version, keep reading this article to learn about how each software is different in terms of the user interface.

Creating A Technology File

So, we are starting with creating a new technology file. If you do not know what technology file is, think of it as an equivalent of Microsoft Word. Every time you write a new article or report in the word processor, you style your text and fonts differently. Similarly, creating a technology file allows you to utilize the same design settings, such as units, grid size, track width, etc., for different projects. This is useful, for example, when you are using the same company for manufacturing and they have their own specifications.

To create a new technology file in DS PCB, go to File - New - New Technology File. A new window will pop up, where you can choose if you want to create a Schematic or PCB Technology File. From Copy From File option, you can select the technology file that you can use to start with.

DSintro_adebe1bd6ea7f8a6514b1612129b3164ac816425.png

Creating a technology file in DS PCB

DSProintro_754415577a2a019153836533db44426ca9f2fafb.png

Creating a technology file in DS PCB Pro

In DS PCB Pro, you will notice that the dialogue window is a bit different. You will see a separate tab called Technology, which has the same options as in DS PCB.

Units

Once a new window for Technology file window comes up, you can start by specifying the measurement unit for your design. In Settings, you have the option of specifying Imperial or Metric units. In DS PCB Pro, however, you can toggle between units using shorthand <Shift-I>, which is very useful when you need to work with both Imperial and Metric units.

DSunit_ae15e7c336045297b3684707b2d1c70ee53bc103.png

Choosing units in DS PCB

DSProUnit_e6e423dba158ec44fe5771c4a108591d7dbf60cd.png

Choosing units in DS PCB

Grids

Grids dialogue comes with more options in DS PCB Pro. You can create and save you own grids with its own display settings. You can also use polar (radial) grids. The Grids dialogue is available through the Settings menu for both software.

DSGrid_1ec419f2a632ef77a377118a2ff8370db7b03b36.png

Grids in DS PCB

DSProGrids_a44d3091b3916014c63f170e1c71bcb09fd325ee.png

Grids in DS PCB Pro

Design Technology

This dialogue is used to define styles for the design. This might include shape and size of pads, text and line styles, connections, etc. Along with previously available settings, you can now define the Hatch style, assign a system Value Name to your components and create Variants of the same design in DS PCB Pro. Other options include adding and modifying Blind and Buried vias in Layer Spans dialogue, assigning which rules should be kept and which are not for the components in Component Rules, and specifying the allowed wire length in Wire Length.

DSDesignTechnology_d253110984dba254b0198a6f53425e15a4433848.png

Design technology dialogue window in DS PCB

DSProDesignTechnology_cc0edd59e9cb02ef97b67fb60181b7f7899a9c58.png

Design Technology dialogue window in DS PCB Pro

Colours

In Colours dialogue you can change the colour of any design item. DS PCB Pro comes with a lot more options for this dialogue as compared to DS PCB. For example, you can now use autofill when creating new symbols such as op-amps. You can also specify colours for Nets and Net Classes. The colour setting can be saved in Colour files and be used again for other designs.

DSColours_98c66cc7dcd3b749acdf8ef2744e6d412f010499.png

Colours dialogue in DS PCB

DSProColours_24bae8da1bdbcc1bbc4b7c173e570dd4c4339d78.png

Colours dialogue in DS PCB Pro

Customise

Apart from defining keyboard shortcuts for commonly used functions, this dialogue in DS PCB Pro allows to edit the Toolbar, Menu and Commands as well as edit some general features in Options. You can customize the user interface by changing the visibility of the Toolbars from the list of available toolbars. In the Menu tab, you can define what type of menu needs to be displayed for different types of design. Lastly, in the Commands tab, you can drag and drop commands that you wish to keep on the toolbars.

DSCustomise_e6a731fd6c839ba4ecf3c5a1efc4be265f4726b8.png

Customise dialogue in DS PCB

DSProCustomise_d3a69a5c56f877961a8d463bdc3e74f0e7fc8367.png

Customise dialogue in DS PCB Pro

Preferences

In DS PCB, you have the option of working with dual screens. In Settings - Preferences - Dual Screen tab, you can specify how you want to arrange separate instances on multiple monitors or on a single large screen. You can also modify interaction features (e.g. mouse sensitivity) separately for schematics and PCB designs. DS PCB Pro comes with a separate dialogue for editing the properties of PCB Tracks. The warnings that are displayed in the application window can be enabled or disabled in Warning tab of Preferences section.

DSPreferences_9436ad9c071981b4f3ffd4fca7f6004382a58719.png

Preferences dialogue in DS PCB

DSProPreferences_519c5b5437b8efc869254245d96bf04602c7296c.png

Preferences dialogue in DS PCB Pro

Schematics & PCB Design

Some of the new features when it comes to the design files are described here. First of all, there are Cutout and Merge options that were not previously available in DS PCB. This is particularly useful when drawing both Schematics and PCB symbols. Secondly, DS PCB Pro now comes with the multi-level hierarchical design. This allows the creation of more structured designs by breaking down a problem into functional elements and tackling each of them individually or so-called “Top-down” approach. Another method is called “Bottom-up”, where the common circuit elements are re-used by saving them in “blocks”. In Settings - Add menu, if you choose Block option, you will be able to specify a block name and the content design. Additionally, the documentation process can be improved tremendously with new features like Bitmap, Design Notes, and Text Callouts being added to your design. Lastly, Schematic DRC, which allows you to perform a large range of checks, including unconnected pins, can now be performed to minimise design error at schematics stage.

DSSchemAdd_bafa9ffb7ecf29a04e99cc6684aa5f457e88fd43.png

Schematics design dialogue in DS PCB

DSProSchemAdd_23d0936a437ce64380a89e57302218fa65c69998.png

Schematics design dialogue in DS PCB Pro

The routing game in DS PCB Pro has improved dramatically. We have another article on DesignSpark that features some of the routing capabilities. On top of that, you can now use Blind and Buried vias in your design. DS PCB Pro has a more extensive set of design rules in DRC dialogue, including thermals and components check. Extra items that do not need to be on the board, but you still want to include them in Bill of Materials (BOM), can be kept in the Associated Parts section. Drill Table and Layer Stack graphics can be added to the design from the Documentation. You can start enjoying the benefits of mass production by accommodating multiple PCB designs on a single layout. This is available through Panel Wizard dialogue.

DSPCBAdd_a7f40f679ff2e593c5fffecb8432d08ba96dbe17.png

PCB design dialogue in DS PCB

DSProPCBAdd_c93ff0320d850bc909263e991b783c0679ab727f.png

PCB design dialogue in DS PCB Pro

driltable_c7a8216df38f4d10103c3a6ead235a9f81babeb8.png

Drill table and layer Stack information in the PCB design

In case you only have access to PCB design files, you can reverse engineer back to schematics containing components and connections which represent the same netlist as that defined in the PCB in Reverse Engineer dialogue. Different versions of the design file can be analyzed in Design Revision Analyzer to find any significant discrepancies. Another useful feature of DS PCB Pro is the ability to include Teardrops and Auto Fanout.

DSTools_64dbf2124133e96a754d3cf2140f001baffc8419.png

Tools design dialogue in DS PCB

DSProTools_28b003d477f1a25b0b51b38172e3526bc8725608.png

Tools dialogue in DS PCB Pro

Have you tried DS PCB Pro already? If so, add a comment below of your favourite and most useful feature.

If not, the free trial version is a great way to try out DS PCB Pro.

DOWNLOAD & INSTALLATION

I am an electronics engineer turned data engineer who likes creating content around IoT, machine learning, computer vision and everything in between.
DesignSpark Electrical Logolinkedin