Skip to main content

Creating perfect COIL SPRINGS using the fastest methods - Techniques and Tips


 

Example: Closed coil Compression Spring.

Creation uses a single helical pull operation showing the quickest method. Tips on the correct use of the Pull tool.

Transition between working and closed coils showing a perfect blend and not a crease - the easy way with tips on selection, trimming blending and combining.

mceclip0_ce8929ca9f06935d40154cd8bb8dd20e3459931a.png

Compression Spring details:

OD 6mm

Wire Dia 0.25mm

2 1/2 close but not exactly closed coils both ends. (0.01mm coil separation)

Overall height 10.6 mm

Other: *Smooth transition between closed and working open coils.

Open coils 1.5mm spacing - 6 full turns

 

* Optional > the fastest way is shown.

 

First sketch out the spring shape:

Information from spring catalogue or from calculations:

 

Create a point at the spring wire center:

The OD is 6mm, so I use 3-0.25/2 or enter 2.875

mceclip3_c428bfd0aa27ac75bd45f947fb6434795b920005.png

 

Calculation to create the closed and working coils in a single Pull (Iterative) command:

Note: The overall height of the coil center line, is the actual spring height less 1x wire diameter 10.6-0.25 =10.35

The full height of the coil consist of 3 sections:

1. Approximated closed Coils > calculate or enter formula 

2. Working Coils 6x1.5mm

3. Approximated closed Coils > enter first result 

 

Select the point > Pull

Select Revolve Axis Z

mceclip4_b88b639b6cf8ed706914bb92ac5ca9a955191f66.png

 

Select Options - Revove helix

mceclip5_3891fc273d7d3dd7d0bbd396b40122112a86a91f.png

In height column, type (10.6-0.25-(6*1.5))/2 > TAB to calculate the closely coiled height (note this value), now type the Pitch value which must be a larger than the wire diameter , say 0.26 ,otherwise the Cylinder thickening process will not be created.

mceclip6_d0c450b5fea2529fb01b45725153b72da3889143.png

Note the Full pull length indicator icon is now active:

mceclip7_191a0c9b2d00a4e33e884a45012cbe98c98f5b4a.png

Select to create the first coil center line wire length section

mceclip8_daf2640006201e9324d1b8a497b86251965a99c0.png

Note the Pull helix command is still active but the pull full height icon symbol is now inactive:

mceclip9_61bc246ba2aa2106d1c91cf8ee78fd6086af0c6a.png

Type the working coil height or the formula 6*1.5 TAB > type the working coil pitch 1.5

Note the Pull full height icon symbol is active - select it to add the working coils.

mceclip10_ca58d187c5e9dc04c33f9a52f0a1c36c8712a7fb.png

 

 

mceclip12_ea3304318ad4ea62c697e8568d031b837b1973a6.png

 

Repeat the first closely coiled section results or repeat the full formula  > Height: 0.675  Pitch: 0.26 > Enter

Note the Full pull icon is active :

mceclip13_e3e671fec6b00eaf253102b769d5f4f8e5bac213.png

 

Check the Z height between the end positions:

mceclip14_da1fbc8cd68d6182fe93acb2dcbf16b4b6a0c53c.png

The full coil consists of 3 sections unjoined (not connected):

 

For a simple spring without a blend transition between the 3 coils:

Box select coils

Select the Cylinder tool

mceclip15_a6f1ce2e4935a2e4e1582fb7e102a37e801fe341.png

Enter the wire radius 0.25/2

Note the kink in the coil will be visible in any drawing view:

mceclip16_52298a28d296cc5ecbeb17e0e35a4b06b6b98afe.png

mceclip19_947d95a561f28b5105f8bbf2f596d75202bd9af3.png

 

If preferring to not have any visible kinks on the model, then the wire helix end sections need to be blended.

First, ADD a point on the curve when it is to be split: Sketch > Enable 3D ( Constraint sketcher) 

mceclip20_9ec3a944f89b7817959c77df776e191b9183d378.png

Usage Tip:

Do not attempt to select 'through' the coil - have the curve ends to be selected at the front of the model.

mceclip21_4cf26210a110312945ba747a06d50dafaa13a334.png

Tab>

mceclip22_68e450aa3d23caf8db513c2511349c014dbe4e25.png

Repeat for touching curve:

mceclip23_6b7797a9c37179f8bad1cf3bc1758ddb40dc4d58.png

mceclip24_5ec4abbddcdd56ee5648924b50896ef2afc49085.png

Now use the Split Curve command from the Sketch tools

mceclip25_f0c2ea5329d291a47c20399909ebefccb16ffa55.png

selecting the curve at the point position to split it

Repeat for all curve ends:

mceclip27_d11699705cd349e68a1accda1419474e9fe9a4c4.png

If creating drawings, place a point at the original curve intersections for dimensioning purposes.

Split the curves and delete the curve end lengths and the points on them:

mceclip29_68b35b111216f9e351b850d2bed348aa62572893.png

 

Select each curve end > key B ( blend)

mceclip30_2cf6187a3682655330a10c076e1a6b0cd250c82e.png

Select the Add Tangent guides

mceclip31_4dec962d06376c83260d6b4b5f628fb3e5ae4fc8.png

or Alt ( Ctrl +Alt) selecting each curve individually

mceclip32_29a647d495d11649377abfeaa62a259b24ec5d8a.png

Comfirm the blend by selecting the green Tick

mceclip33_ec55cc2dc6be59bb2f158ed980243f0cb7e0fc74.png

Join up all the 3 helix sections and the 2 curve blends:

Select the first insecting coincident curve end position > Fill (key F/f), repeat by pressing the key F/f to complete. The whole coil is now a single spline as shown.

 

If a drawing is required, it is important to rename the points:

mceclip34_c1139d2ff2c0b52d9f1eac80e111fbdf16b88026.png

Finally to add thickness to the center line curve, select it, then select the Cylinder tool from the Design Tab - Insert menu

 

mceclip35_e2e933aaef8f46f793aa3361282372394014425d.png

Enter the wire radius

The transition sections are tangent:

 

A Detail drawing can be made:

Model points and a circle are required to create dimensions (requiring renaming). Helix spline surfaces can not be otherwise dimensioned.

mceclip0_d5256c7ef1d456b5909ca9bfe41c59d9667752b0.png

With practice, the coil spring can take only 4 minutes to completely model with transition blends as shown or less without the blends.

Comments