Skip to main content

Although Raspberry Pi 4 has been released, should you upgrade? To what extent does it improve upon the Raspberry Pi 3B+, and should you consider purchasing one rather than waiting?  

For as little as $35 for a 2GB variant, you can use Raspberry Pi 4 as a kids' learning PC, video centre, web server, video game emulator, or as a robot or IoT device's brain. It reveals many opportunities for improving life and enjoying a great time. Since the Raspberry Pi 2, the Raspberry Pi 4 is the most significant update to a previous edition. This article will update you on things concerning the Raspberry Pi 4 like the Raspberry Pi 4 pinout.

Impressive Raspberry Pi 4 Specs

Raspberry Pi

The upgraded system specification is the primary motivator for purchasing the most recent Raspberry Pi model. This is what you'll discover:

  • H.265 (4Kp60 decode)
  • USB-C power
  • Power-over-Ethernet (this will require a PoE HAT)
  • Micro-SD card slot
  • OpenGL ES, 3.0 graphics
  • On-board Bluetooth 5.0, low-energy (BLE)
  • H.264 (1080p60 decode, 1080p30 encode)
  • CSI camera port
  • DSI display port
  • Gigabit Ethernet
  • Combined composite video jack and 3.5mm analog audio
  • 2× micro-HDMI ports (up to 4Kp60 supported)

How Does Raspberry Pi 4 Improve on Other Models? 

Several notable improvements include a faster processor (CPU and GPU both clock in at 1.5 GHz from Broadcom), more extensive and quicker RAM, more USB 3 connections, dual mini HDMI ports (rather than one HDMI connection), and 4K output support. The onboard Ethernet connector may now support genuine Gigabit connections of 125 MBps. In contrast, last-generation versions could only theoretically support 41 MBps due to the more incredible bus speed that allows USB 3 functionality. Additionally, its microSD card slot is two times faster than the 3B+, with a maximum speed of 50 MBps instead of 25 MBps.

You can charge the Raspberry Pi 4 B via USB Type-C rather than micro USB because the upgraded SoC requires more power. It also needs a power supply that can provide a minimum of 3 amps and 5V, though if you only have a few USB-connected accessories, you can get by with 2.5 amps. Aside from the power requirements, the reversible nature of USB Type-C connectors makes them considerably simpler for adults and children to plug in.

The Raspberry Pi 4 is an entirely new platform, yet it shares the same shape and size as its predecessor thanks to the Broadcom BCM2711B0 chip. All previous Pis utilized 40nm SoCs since the original in 2012; this chip, however, is built on 28nm technology and employs the newer Cortex-A72 microarchitecture. At first glance, the quad-core, 1.4-GHz BCM2837B0 in the Raspberry Pi 3B+ doesn't appear to be significantly faster than a four-core, 1.5-GHz BCM2711B0 featured in Raspberry Pi 4.

Instead of awaiting the outcome of a process before beginning on another, the Cortex A72 offers out-of-order execution. It has a 15-instruction pipeline depth compared to the earlier model's 8-instruction pipeline depth. Therefore, Cortex-A72 processors become faster and consume more power compared to their A53-powered progenitors even running at the same clock speed (although the BCM2711B0 is predicated on a lower manufacturing node).

For instance, the Pi 4 completely crushed the Pi 3 B+ in each test on the Linpack benchmark, which gauges total processing power. The Pi 4 outperformed the Pi 3 B+ by 413%, scoring 925 instead of 224 on the pivotal single precision (SP) test.

Additionally, the RAM is much faster, going from the Pi 3B+'s 1GB of DDR2 RAM to the Pi 4's up to 8GB of DDR4 RAM. Extra RAM is essential, especially for web browsing and higher bandwidth.

The GPU also received a significant upgrade, transitioning from a VideoCore IV with a 400 MHz core clock speed on the Pi 3 B to VideoCore VI with a core clock speed of 500 MHz. Thanks to its updated internals, it can now support two displays at 4K resolution and 30 fps each, or it can output at 4K at 60 fps to a single display

Updates on Raspberry Pi OS

update on Raspberry Pi OS

With the most recent update, several new desktop improvements have been added to the Raspberry Pi OS, which boosts text-based search, network administration, and camera system access.

In addition, a text-based search box has been added to Raspberry Pi OS for locating programs like File Manager, the OS Imager, and the Image Viewer. By tapping the Windows key on some keyboards or the Raspberry key on this one, you can access it. The current menu is still available.

Additionally, an icon for audio input and output has been added. Adding a USB or Bluetooth audio device also triggers the appearance of a microphone icon.

Ctrl-Alt-W and Ctrl-Alt-B are two new keyboard shortcuts for launching the Wi-Fi and Bluetooth menus, respectively.

The software NetworkManager, which is well-liked in other Linux distributions for managing Wi-Fi networks, is included in this release. Up till now, Pi OS used dhcpcd to control Wi-Fi network connections. Users must enable NetworkManager in addition to the standard dhcpcd. But in the future, it will be the standard. The two systems wait to transfer connections. Users must also reset any customized network settings.

Conclusion

If you're in the market for a low-cost but high-quality single-board computer, look no further than the Raspberry Pi 4. The Raspberry Pi 4 can perform desktop computer tasks, though most adults wouldn't want to.

The people who use Raspberry Pi 4s instead of x86 PCs do not, however, reap the most significant rewards from the Raspberry Pi's performance and ample RAM; instead, it's the innovators who employ that power to develop new Internet of Things (IoT) gadgets, servers, and robots.

LindaWelsh has not written a bio yet…