DesignSpark フォーラム
このフォーラムでは、世界中のDesignSparkに登録しているメンバーと様々な技術的相談や、議論を行うことができます。また、自身のアイデアに賛同してくれるエンジニアを、世界中から探すこともできるでしょう。
英語の投稿が目立ちますが日本語の質問でも問題ありません。よく海外から片言の日本語で回答を頂いたりします。自動翻訳レベルでも結構ですのでグローバルなユーザとのコミュニケーションをお楽しみください。
This is just an example of using blend to make a varying blend ( R5 ~ R15 ) between two complex spline irregular surfaces.
First make an intersection curve between the faces. At each end of the spline curve, sketch either the small or large circle. Blend between each circle using the intersection curve as the center line path making a wavey varying diameter cone along the final edge. Cut each surface using the same solid edge cone. Finally, blend between the surface edges with tangency.
Tangency angles are good at approx 0.02 degrees
Of course it's not automatically made, but the end result is visually beautiful and accurate.
https://www.rs-online.com/designspark/mission-responsible-coming-soon-new-podcast-series
For those here who celebrate Easter, why don't you enjoy the long weekend with an episode of our
Mission:Responsible podcast? Episode 6 is out now!
The assembly can have a face moved / pulled etc with the open component and the drawing section view window tabs simultaneously updating - all annotations updating.
Window tabs can be dragged off the DSM application screen to display them, then they can be docked into the main DSM window.
Bonjour,
S'il vous plait je voudrai déplacer les connecteurs vers le haut pour faire grandir la largeur du PCB on respectant les régles de routage, par-ce que lors je translate les connecteurs; les pistes faisons des courts-circuits. Mon intéret c'est d'agrandir la taille du PCB de 160mm vers 214.63mm.
Merci d'avance. 寸法の単位 mmは消せますか? Version 6.03 of DesignSpart Mechanical Engineer.
I open export option :
choice "DXF"
valide .
I see one file *.dxf is make but it is empty.
it is some issue with DXF export?
what upset I need ( file empty perhaps I have missing )?
Bonjour,
S'il vous plait, comment modifier la longueur ou la largeur d'une PCB à condition que je garde les méme pistes et méme les pads comme il faut.
Merci d'avance. Ich versuche, zwei markierte Objekte aus einem Projekt in ein anderes zu kopieren mit String c und String V.. Leider tut sich in dem anderen Projekt gar nichts, wenn ich dies aktiviere und mit String v drücke. 図面で点間の寸法が定義できない。
例えば六角ボルトの頭で長手方向で寸法が記載できない I'm trying to understand the DRC errors I've been given. I don't really know how to tell what text is considered to be on the silkscreen and what is just indiciating pin information. The schematic/pcb files I downloaded for the ESP32-WROOM-32E was said to be verified by SnapMagic (ESP32-WROOM-32E (16MB) footprint & symbol by Espressif Systems | SnapMagic Search (snapeda.com). This is my first PCB I have created and am struggling to understand how to fix the issues. Hello, people
I worked hard couple months on this project and in some time i made a mistake with the geometry and the solid has tirned into surface. Cannt work with this anymore.
Please, is there any chance to fix it and return to solid back? Just an example to show some capability - done in 6.0.2 The idea came from a Fusion 360 online video.
DSM although basic in tools can still accomplish some decent shapes with good blends and edge rounds. The zebra strips show good surface transitions handled by the Parasolid kernal.
DSM can't descriptively do G2 surface continuity, but for practical purposes for many molding purposes this is accurate surface modelling.
Note the strips transitioning over the surface edges...
Multiple Zebra views on Drawing sheet
Drawing with the guiding principle curves:
To refine the shape, modify the layout curves and re make the surfaces.
The new universal Instant mirror tool is very handy - good tangency over the reflected handle halves
See the zebra strips:
Ich bekomme dauernd nachdem ich eine Ebene mit Text (nach Bemaßung) Versuche auf einen Körper zu projizieren die Meldung keine Rückmeldung und das Programm stürzt ab. Hat das etwa etwas mit Version 6.0zu tun ? I have just upgraded to Creator and still do not have access to a New Drawing Sheet selection. It is like the software does not know that I have upgraded even though I have reset the license and relogged in. Please help. Thanks, Jonathan There seems to be an odd isue when exporting my design to STL
This is what the basic design looks like - a cylinder with internal threads.
When i export to STL or Cura, this is what i get
If i slice it, it wants to print it as a sold.
Anyone have any ideas?
I've attached the rsdoc if anyone wants to look at that
最近のフォーラム投稿
Variable blend ( R5~R15) between complex irregular spline surfaces - sample
Nothing to do on the long Easter weekend? Listen to our podcast
Viewing multiple Window Tabs simultaneously - how to create and dock
Modifier la largeur du PCB
寸法の単位 mmは消せますか?
Can not make a DXF file
Modifier la longueur d'une PCB
Wie kann ich markierte Objekte von einem zum anderen Projekt kopieren?
図面で点間の寸法が定義できない
Confusion on Silkscreen Error
Solid has turned into Surface :(
Surface Modelling - Handle shape
Projizieren funktioniert nicht mehr in Version 6, warum nicht??
New Drawing Sheet
STL Exporting gone awry