How do you feel about this article? Help us to provide better content for you.
Thank you! Your feedback has been received.
There was a problem submitting your feedback, please try again later.
What do you think of this article?
The emerging commercialization of Unmanned Aerial Vehicles (UAVs) otherwise known as drones are all controlled by Radio Frequency (RF) wireless communication links. One needs to understand the frequency bands that are available and the trade-offs. The issues of data rate, types of data (control, packets, video, audio) both real-time and time-delayed based as well as range due to output power and in-flight durations must all be considered concurrently as these factors will determine the choice of available options.
I was researching some of the drone UAV / Quadcopter / Multi-copter Wireless (Telemetry) Communication Links frequencies to see what was available and came across the APM 2.6 module which lead me to their telemetry options landing page :
https://ardupilot.org/copter/docs/common-telemetry-landingpage.html#common-telemetry-landingpage
In reviewing all of these I was able to 'boil down' these types of wireless communication protocols and their typical maximum distance at 100 mW of output power and clear line of sight using an omnidirectional monopole antenna with 2.15 dBi of gain:
- Bluetooth (up to 100m with Class 1)
- Wi-Fi (up to 100m at 2.4 GHz and 50m at 5.6 GHz)
- Wi-Fi 4 using MIMO (up to 200m at 2.4 GHz and 100m at 5.6 GHz)
- ISM (Industrial-Scientific-Medical) 900 MHz UHF Band (up to 2 Km)
- 4G / WiMax cellular (up to 4 Km)
- 5G cellular (up to 1 Km at 5.6 GHz)
Also, all distances are nominalized using the same data rate, but since lower frequency bands typically handle lower data rates, they are able to handle longer distances using the same output power.
However, for First Person Video (FPV) control where the data is much higher and streaming real-time, distances can be much shorter before the data stream starts to fragment and frame error loss increases logarithmically.
So when considering your wireless link to your drone, you must consider these usage model criteria to balance your choices :
- Output power
- Antenna gain
- Frequency band
- Data rate
- Elevation
- Operating time
One of the best ways to increase range, especially for higher data rates and to reduce power (longer flight times) is to use a MIMO multiple antenna approach. Another is to use an extremely high gain antenna, and finally, the best way is to use a directional tracking antenna.
Each of these adds a higher level of complexity as well as increased costs, but for top performance, each must be weighed carefully.