Skip to main content

Simplify the design of semiconductor relay functions! - Panasonic MOSFET Driver Vol. 2

This article introduces "MOSFET driver" of Panasonic serialized.

The previous article (Vol. 1) gave an overview of the MOSFET driver.

In this article (Vol. 2) and the next article (Vol. 3), Panasonic will introduce you to the high output voltage and high-speed operation required for driving Si-MOSFET and SiC (Silicon Carbide) MOSFET. Here are some suggestions for you.

Panasonic High Power MOSFET Driver (NEW)

See Panasonic's MOSFET driver lineup here

Read more about DesignSpark (Panasonic MOSFET Driver, Vol. 1)

Power MOSFETs used in power supply applications such as industrial equipment, information infrastructure, and power storage systems are currently the mainstream for Si-MOSFET.

In addition, SiC (Silicon Carbide) MOSFETs, which are being used not only for automotive applications but also for industrial applications in recent years, are becoming increasingly popular.

High output voltage and high-speed operation are key factors in obtaining high driving efficiency.

In this article, we will introduce solutions to achieve "high output voltage.“

Case 1: Reducing the On-Resistance of a MOSFET by applying a high voltage (Vgs) between a gate and a source

I want to apply a large voltage between the MOSFET gate and source

Before

The output characteristics of this SiC-MOSFET are attractive.

However, to reduce the On-Resistance sufficiently, it seems that I would need to use two conventional MOSFET drivers. I do not want to increase the area occupied by adding a second driver.

arrow

This is possible with the new Panasonic MOSFET driver!

Vgs = Typ. 18 V can be applied. I can sufficiently lower the on-resistance of SiC-MOSFETs!

After

With the new Panasonic MOSFET driver, I can reduce the On-Resistance of this SiC-MOSFET and be able to supply the necessary voltage using only one!

Even when using a MOSFET with a high gate voltage such as SiC, a high output voltage type is safe to use

【Recommended products】 MOSFET Driver High Output Voltage Type

MOSFET

【Reason for Reccommendation】

High output voltage contributing to reduction of MOSFET on-resistance. It is also possible to drive MOSFETs with high gate voltages such as SiC.

Type High Output Voltage
Part Number APV 3111 GVY
Short Circuit Current (Isc) 12µA
Open Output Voltage (Voc) 18V

Catalog download

CAD data download

【Advantages】 Small high-output voltage

For full performance, such as when using SiC MOSFETs.

For MOSFETs requiring a high gate voltage Vgs. Small size can supply sufficient voltage.

【When using a conventional MOSFET Driver】

MOSFET driver

Operation is possible with the supply voltage from the driver, but the On-Resistance will not decrease. Two MOSFET drivers are necessary to increase the supply voltage.

【When using a high output voltage type MOSFET driver】

When using a high output voltage type MOSFET driver

One MOSFET driver can operate SiC-MOSFETs. On-Resistance can also be lowered sufficiently!

Please consider Panasonic's MOSFET driver with high output voltage for applications that require power circuits such as industrial, robotics, telecommunications/infrastructure, and automotive applications in order to achieve high output voltage.

In the next article, we will look at some of the suggestions you can make to meet your “fast” switching needs.

Pearls of WISDOM on Automation Controls

Please check useful information for engineers from the basics of control equipment to applications!

Panasonic Industry Company contributes towards a new future and a richer society by providing various high quality and reliable industrial products. On DesignSpark we will introduce new products and provide technical information. パナソニック インダストリー社は、新しい未来と豊かな社会に貢献する会社を目指し、高い性能、信頼性を実現した商品を多数扱っております。DesignSparkでは弊社商品や技術記事についてご紹介いたします。