Skip to main content
The main purpose of this project is to design a system in which the number of persons entering or leaving the store is tracked and detect their temperature. Then, displayed on the screen (LCD).

Pandemic Surveillance System

This project describes the design and work of a Pandemic Surveillance System. The main purpose is to design a system in which the number of persons entering or leaving the store is tracked and displayed on the screen (LCD). When someone enters the store, the count would be increased and the buzzer will sound, whereas on leaving, the count would decrease and the buzzer will sound too. PIR sensing mechanism is used to sense the presence of visitors and the entire counting operation is completed by Arduino. Next, the vibration motor is used to inform the users by vibrating on receiving signals. Based on our project, when a user or customer passes through the door, the vibration motor will vibrate and this shown to indicate that someone is entering the store. The next component used in this project is a temperature sensor. Temperature sensor functions as an electronic device that measures the temperature of environments and converts the input data into electronic data in order to record monitor or signal temperature changes. In our project, the temperature sensor is used to detect the temperature of visitors entering the store while the buzzer will sound to indicate the level of temperature of the visitor. For example, when the temperature of visitors is too low and too high, all the led will be light up, all the buzzers will sound and it is stated as a none valid temperature. Next, when the temperature is good, the green led will be light up and the buzzer will sound, when it is moderate, the yellow led will be light up same goes as the buzzer, and lastly, when the temperature is high, the red led will be light up and the buzzer will sound. Lastly, the current visitor and the temperature result will show on LCD.

1.1 Temperature Measurement

Table 1.1

TEMPERATURE (0C)

LED LIGHT
< 35

Green, Yellow, Red

- Not Valid -

35 - 37 Green
38 - 39 Yellow
40 - 43 Red
> 43

Green, Yellow, Red

- Not Valid -

2.0 Circuit Diagram

pss_full1_05c1b4887e515c4600ca909bfe54055719c1a7c8.png

 

Diagram 2.0: Full circuit

3.0 The Diagram of Simulated Project

1.1_2_e7896d5129f94a1fff2c2f20aa92921f365d7729.jpg

 

Diagram 3.1

Start simulation.

2.2_1_e7210877d16045002ef9b6a42839941da576ce9c.jpg

Diagram 3.2

The LCD display number of visitors.

3_%282%291_7ea4e2acbcfe11ad500d8c1ddd99d3bf1f31302a.png

Diagram 3.3

The LCD display temperature of visitors.

4_%282%291_e8dee68c9fefce8932233817ae40094a386c9f97.png

Diagram 3.4

The PIR sensor sensing visitors, piezo will sound.

558_043ac107682f23b7708544fdf1db4fe506409be5.jpg

Diagram 3.5

The Vibration Motor will vibrate.

643_60944ded1bb975a1a64e07bccf1fcb1c195ebc6e.jpg

Diagram 3.6

The temperature sensor works.

When temperature < 35, all LED lights up and piezo will sound.

731_5a75ebccb1e92dd20e1f8b0873c99bac9b27a8d4.jpg

Diagram 3.7

The temperature sensor works.

When temperature >= 35, LED green lights up and piezo will sound.

828_2afcce35dc11bbef77e92ec54c59ef821f9b2a41.jpg

 

Diagram 3.8

The temperature sensor works.

When temperature >=38, LED yellow lights up and piezo will sound.

923_58e0c1320c00f21926dddd6df571cfff2143dd1e.jpg

Diagram 3.9

The temperature sensor works.

When temperature <= 42, LED red lights up and piezo will sound.

1047_237e98d0538dd7c74b504d645e4c7ca8d6ac709d.jpg

Diagram 3.10

The temperature sensor works.

When temperature <= 46, all LED lights up, and piezo will sound.

11_%282%29_1b5058b48341daa9b067321e06dfe70085a42a1f.png

Diagram 3.11

People in, visitor count 1.

LCD displays total visitors and “PLEASE VISIT”.

1253_4f598913c1de189bf401b1a8b92d8aa9558ef0c4.jpg

Diagram 3.12

After that, the LCD displays the temperature of

the visitor.

13_%282%29_b8b6e1dc0b6001fa44cdbf3078c536a09c40317c.jpg

 

Diagram 3.13

People out, visitor -1.

LCD display.

1445_4f598913c1de189bf401b1a8b92d8aa9558ef0c4.jpg

 

Diagram 3.14

When people out, the LCD display temperature of the current visitor.

1542_79a5fc0e780aca774ead849b08b34728f8efe3ad.jpg

Diagram 3.15

LCD display “PLEASE WAIT”

If total visitor =10 and buzzer will sound until

the number of visitors = 9.

4.0 Tinkercad URL Link of Design Project

https://www.tinkercad.com/things/3wYVimVCgAP-assignment-benr-1812-s1/editel?sharecode=ymTgpFweNH5LAMQRcWvQ9x1Rz_I5yiPHqRJOfJIDS5s

Downloads

ADIBAH ARIFIN has not written a bio yet…