Skip to main content

ESD suppressor for high-speed communication network: Proposal to those seeking electric discharge (ESD) control for automotive Ethernet!

ESD suppressor is the component used to eliminate electric discharge from the circuit and transfer it to the ground.

 

The internal structure of an ESD suppressor entails a cavity, the resistance of which significantly decreases when a high voltage is applied. Consequently, ESD suppressor protects the electric equipment from static electricity. In normal conditions, however, the signal is not affected as the resistance value of the ESD suppressor is very high.

 

Constructions

Functions of ESD suppressor

V-I characterristics of ESD suppressor


How to use

Implementing an ESD suppressor is very straightforward. Connect the ESD suppressor between the signal line and ground just below the connector (IF). In the case of BCI (Bulk Connect Injection) testing, a CMNF is required in the differential signal lines to eradicate electromagnetic noise. Using an ESD suppressor between the connector and CMNF helps suppress both static electricity and electrical noise and result in high-speed communication.

Position of ESD suppressor

 

Comparing with TVS Diode

There are two types of components for ESD control, ESD suppressor and TVS diode. However, in the case of BCI testing for automotive Ethernet, using a TVS diode has its limitations. On the contrary, ESD suppressors can be placed directly after the connector, as shown in diagram ESD_1. Additionally, as shown in diagram ESD_2, TVS diodes need to be placed between the CMNF and Ethernet PHY, which consequently decreases the ESD protection capability and causes communication errors. Details here.

Component placement ESD2

Component placement:(ESD_1) Connector-ESD-CMNF-PHY

Component placement ESD2

Component placement:(ESD_2) Connector-CMNF-ESD-PHY

Product Introduction

Panasonic’s ESD suppressor is high withstanding type according to AEC-Q200. (in-vehicle electric equipment ESD standard ISO 10605, atmospheric discharge 25kV) Moreover, because of the small electrostatic capacitance (0.1pF) and high rated voltage (DC50V), the risk of communication errors due to noise is negligible. Therefore, Panasonic ESD suppressor is highly suitable for automotive CAN and Ethernet.
ESD Suppressor, High withstanding type.

Panasonic Industry Company contributes towards a new future and a richer society by providing various high quality and reliable industrial products. On DesignSpark we will introduce new products and provide technical information. パナソニック インダストリー社は、新しい未来と豊かな社会に貢献する会社を目指し、高い性能、信頼性を実現した商品を多数扱っております。DesignSparkでは弊社商品や技術記事についてご紹介いたします。