RE : [DesignSpark by RS Components] Re: I can't run DSPcb 8.1 is unable to verify authorisationmasquer
Dominique TERRIER s.e.d.i.m@wanadoo.fr
samedi 4 avril 2020 à 19:54
envoyés
DesignSpark by RS Components support+ <id8129@designspark.zendesk.com>
Hello John,
I can not confirm anything, because when I launch DSPCB 8.1 it displays a 1st window with "Error - Unable to verify registration - OK" after 2nd window with "Error - DesingSpark Pcb is unable to verify authorization - OK" and finally a 3rd window with "Error - DesingSpark Pcb must be authorized in order to continue - OK "AND It's Over
On my DesignSpark account "The DSPCB is activated" and validated green.
My computer is old with a Window XP PRO SP3 Intel I 5 uP system - 3.40 GHz - 4 Go RAM
Internet connection is correct with Norton security antivirus, I don't use PROXY.
With or without Norton Antivirus and FireWall DSPCB does not work.
I don't understand because before DSPCB 8.1 work very well. Do you have any idea of the problem.
Thanks in advance. Best regards. Dominique.
On my DesignSpark account "The DSPCB is activated" and validated green.
My computer is old with a Window XP PRO SP3 Intel I 5 uP system - 3.40 GHz - 4 Go RAM
Internet connection is correct with Norton security antivirus, I don't use PROXY.
With or without Norton Antivirus and FireWall DSPCB does not work.
I don't understand because before DSPCB 8.1 work very well. Do you have any idea of the problem.
Thanks in advance. Best regards. Dominique.
Le : 04 avril 2020 à 10:17 (GMT +02:00)
De : "DesignSpark PCB (DesignSpark by RS Components)" <support@designspark.zendesk.com>
À : "TERRIER Dominique" <infos@sedimee.com>
Objet : [DesignSpark by RS Components] Re: I can't run DSPcb 8.1 is unable to verify authorisation
##- Please type your reply above this line -##Your request (8129) has been updated.
To add additional comments, reply to this email.
DesignSpark PCB (DesignSpark by RS Components)
Apr 4, 09:17 BST
Hello Dominique,
Can you confirm the program has a serial number and an activation key, Go to Help - About and check that window.
Paste a copy of the serial number text into the ticket if the activation code is missing.
It may be that the DSPCB activation and the server have become out of sync, if so I will send a utility to un-register the program and allow you to reactivate.
Kind regards
John
TERRIER Dominique
Apr 3, 22:06 BST
Hello,
I can't run DSpcb 8.1. Problem is registration. Before DSpcb was running without problem.
Thx for your answer.
Best regards.Dominique Terrier.
Regards
DesignSpark Support