How do you feel about this article? Help us to provide better content for you.
Thank you! Your feedback has been received.
There was a problem submitting your feedback, please try again later.
What do you think of this article?
Hello friends, I hope you all are having fun in your lives. In today's tutorial, I am going to give you a detailed overview of this amazing shift register 74HC595. It must have happened to you that you are working on some project and you have to interface many LEDs etc with your microcontroller and at some point, you have no pin left for more LEDs. At that point, this shift register 74HC595 comes handy. 74HC595 is used to increase the output pins of your Microcontroller.
If you are new to this shift register then I would suggest you to have a look at 74HC595 Pinout and download its Proteus Simulation.So, let's have a look at its basic details:
Basics of 74HC595
- 74HC595 is a shift register which works on Serial IN Parallel OUT protocol.
- It receives data serially from the microcontroller and then sends out this data through parallel pins.
- We can increase our output pins by 8 using the single chip.
- We can also connect more than 1 shift register in parallel.
- So, let's say I have connected three shift registers with our microcontroller then our output pins are increased by 8 x 3 = 24.
- I hope I have cleared the idea, so now let's have a look at its pinout.
74HC595 Pinout
- As you can see from the figure it has below pinouts:
- Pin # 1 to Pin # 7 are Output Pins Q1 - Q7.
- Pin # 15 is also Output Pin Q0.
- Pin # 8 is Ground.
- Pin # 9 is Q7' (OutPut Serial Data).
- Pin # 10 is Master Reset.
- Pin # 11 is SHCP which is short for Shift Register Clock Input.
- Pin # 12 is STCP which is short for Storage Register Clock Input.
- Pin # 13 is OE which is Output Enable.
- Pin # 14 is DS which is Serial Data input.
- Pin # 16 is Vcc where we have to supply the power +5V.
- You can quite easily interface this shift register with different microcontrollers such as Arduino, PIC Microcontroller, Atmel etc.
Applications of 74HC595
It has a wide range of applications, especially in LED Boards. You must have seen the large LED boards where we have to control a lot of LEDs with a single microcontroller, 74HC595 is used in such projects a lot.
I hope you will like this article, let me know if you have any questions about this shift register and I will surely help you out. Thanks for reading, take care, bye bye !!! :)