Skip to main content

The Red Tin Audio Expander Part 2: Researching Active Matrix Mixers and Building an Op-Amp Circuit

top10_cde90c77f64791a54395d9d8223b847253fbe0a4.jpg
Researching and building an Audio Op Amp to be incorporated into an active matrix mixer

I previously built a passive matrix mixer that I named the Red Tin Audio Expander and the blog post attracted quite a few helpful comments, mainly suggesting that to be properly effective, it needed to be active design rather than passive.

This post takes a look at a first attempt at building an active matrix mixer with op-amps. I also decided to scale down this down slightly to 3x mono channels, plus a stereo in/out for the Red Tin send and return. This should make the build slightly more manageable.

Op-amps

op-amp3_57c3bf1110f451a1616e01be936264a95cf11e4b.jpg
Reading up on active matrix mixers and taking into account some of those comments on my passive design, I worked out that I was going to need an amp for each input. As DesignSpark member 44meurope put it, “an (op)amp for every input, and (summing) op-amp for every output”.

I have tried building audio op-amp circuits in the past and for some reason encountered a few issues, so I thought I should do some more research to get a better understanding of what I was dealing with.

Simply put, an operational amplifier (usually referred to simply as an op-amp) is a device to amplify voltage. My reading up taught me that, at their most basic, an op-amp takes a differential signal — the voltage difference between the V+ and V- pins — and outputs a voltage proportional to this difference via the Vs+ and Vs- power supply.

This “open-loop” operation typically results in a device gain (known as the open-loop gain or AOL) of 100,000 or more. Even a tiny difference in the voltage between the V+ and the V- pins works out to an output of nearly the supply voltage when the plus input voltage is greater than the minus input. This configuration acts as a comparator, turning a potentially varying input signal to a steady on/off output.

Op-amps are more usually used in a closed-loop configuration, with the output voltage feeding back into the inverting input to form a more controllable signal amplification. The simplest way to accomplish this is to use a buffer circuit, where the output feeds back into the inverting input with no resistors or other components.

I discovered that there are two op-amp golden rules:

  1. The output attempts to make the voltage difference between the inputs zero
  2. The inputs draw no current

So, to construct a closed-loop op-amp you need to feed the input voltage into the V+ input, connect the V- to the amplifier’s output and then the output should go to the same value as the + input to keep both equal.

This configuration can be used for weak signals that require an amplified output – which is what I wanted for my mixer and an Internet search turned up lots of schematics for audio op-amps that employed this principle.

Putting theory into practice

breadboard2_2390f89e3a65b6581a42dc1aa9b0a3d7d43f05ab.jpg

As mentioned above I had found quite a few schematics on the Internet, including a couple of plans for Eurorack matrix mixers (here and here) that I had come across when I was building my synthesiser.

The example schematic from York Modular which is shared here was particularly useful (I even ended up buying one of their PCBs to build one for my synthesiser).

I could see the TL082 (304-217) is used in many of these examples and so I decided that is what I would base my circuit on. The TL082 follows the common pin arrangement for dual op-amps:

dual-op-amp-pin-out_7ce8cfe93bc2464760687d118ac2c3104ec663ad.jpg

After trying out various of the circuits on a breadboard, I ended up deciding upon the schematic I found here

audio-op-amp-schematic_02340ad82a24dad9387b9f79bd09bfdfe3f769bc.gif

Using this arrangement I managed to make a simple circuit for an inverting audio pre-amplifier.

Bearing in mind that I am in no way a professional analogue electronics engineer, after my research outlined above, my understanding is that R3 and R4 resistors act as a voltage divider to make 1/2 the supply voltage. For that reason, the two resistors need to be equal. The capacitor between the two resistors is there to filter out any ripples in the power supply and other noise.

The gain of this circuit is determined by resistors R1 and R2 and is calculated by the following equation:

Voltage Gain = R2 / R1

I also read various discussions and articles on the pros and cons of inverting vs non-inverting amplifiers and did not really come to any clear indication of which would be most suitable. In the end, I noted that non-inverting amps seem to be by far the most commonly used in all the mixer schematics I had looked at, so I decided to go with that. So I then modified my original circuit utilising the other half of my dual op-amp to produce a non-inverting amplifier.

oscilloscope-invsout_bcfafef7f504310eb2be8676a4c45e13a4531dcb.jpg
You can see above the input (blue) compared with the output (red) with the potentiometer turned about halfway to full clockwise.

The circuit I arrived at uses the following components:

Resistors

Polyester capacitors

Electrolytic capacitors

Op Amp

  • 8pin DIL socket (674-2435)
  • TL082CP op-amp (304-217)


Next steps

breadboard1_92e0a05798b5f7d30171274de0f49712cd07160d.jpg
My next job will be to transfer the amplifier circuit to stripboard and build enough of these for my mixer. I then need to work out how to connect them to my grid of potentiometers and inputs/outputs, before fitting it all into a suitable enclosure.

I have a background in the arts, environmental conservation and IT support. In my spare time I do a bit of DJing and I like making things.