How do you feel about this article? Help us to provide better content for you.
Thank you! Your feedback has been received.
There was a problem submitting your feedback, please try again later.
What do you think of this article?
Description of operation
In a linear power supply system, mains power is supplied to the transformer via input filtering, which helps to provide immunity from mains-borne noise whilst also reducing emission back into the mains supply. The AC voltage output from the transformer is rectified, before being filtered to remove ripple, which is typically achieved using one or more electrolytic capacitors.
A regulated linear power supply also has voltage regulation in order to maintain a constant output voltage as the AC input line voltage and load current varies. Unregulated power supplies do not have this and their output voltage can vary by a much greater degree.
Protection is optional and can protect both the power supply and connected equipment from faults in either of these.
Pros and cons compared to switch mode power supplies
- Pro: Simpler and more robust
- Pro: Easier to design and maintain
- Pro: Low noise – suited to noise sensitive applications*
- Pro: Typically faster transient response times – therefore may be better suited to more dynamic loads*
- Con: Larger and heavier
- Con: Less efficient if regulated
- Con: Can be more expensive
*Switch mode power supplies are available and can be designed for certain specialist requirements, e.g. use with low noise circuits and inductive loads such as motors