DESIGNSPARK FORUMS
Communicate freely with other DesignSpark members via the forums area. Create new conversations or join existing discussions about products, technology, software, and future innovation.
Help to provide solutions or seek answers to your own technical problems by calling upon a global network of like-minded engineers.
People have tuened to SDR receivers if they want to explore radio communications, propagation or interesting radio signals from round the world. SDRplay RSP receivers are a popular, UK manufactured choice with good customer service and support.
They cover 1kHz to 2GHz as a communications receiver when used in conjunction with free software supplied by SDRplay for Windows, MacOS, Linux and Raspberry Pi.
However thanks to Australian software developer Steve Andrew, they can also become excellent, calibrated spectrum analysers! Steve has just launched a new version of his Windows-based Spectrum Analyser software which includes a tracking generator.
There's a brand new Website with documentation and support information over on https://www.spectrumanalyser.co.uk/
HiI specifically bought a subscription to import OBJ files. But this feature never showed up.
What is the problem? 図面モードで破断にした時 破断面の線を直線からジグザグ線に変更しようと
ファイル→Design Sparkオプション→図面→一般→ラインスタイルのオプション→破断ビューのクリッピングエッジを変更しても変化有りません。知っている方が居られたら宜しくお願い致します。 Bonjour,
Dans une Pcb le courant qui circule c'est entre 100 µA et 2 A .
Est ce que les pistes de class signal est suffisant?
Si non, comment je peux changer la classe liste des pistes pour avoir une class power?
Merci d'avance.
Moderators Translation:
Good morning,
In a PCB the current flowing is between 100 µA and 2 A.
Are class signal tracks sufficient?
If not, how can I change the track list class to have a power class?
Thanks in advance. Bonjour,
Est ce que cette Pcb contient 4 couches?
Si oui; comment je supprimer les autres 2 couches ?
Et qui est les couches qui sont pas utilisé pour le supprimé ?
Merci d'avance
Moderator translation:
Good morning,
Does this PCB contain 4 layers?
If yes; how do I remove the other 2 layers?
And which layers are not used for the deleted?
Thanks in advance I would like to create two objects from one,possibly with "clip with plane". I want an upper half and a lower half. can someone help? Morning, I restored a complete backup from my old (now defunct) laptop to a new laptop. DSPCB will not start and I get a message shown in the attachement below. Can anyone help please. (DSPCB still works perfectly on my main PC). Thanks in advance winodws10では正常に動作していましたが、windows11にアップグレートしてからは、DesignSpark Mechanicalを起動するとエラー表示してスタートしません。FAQを見ても1,2,3,5を確認しても解決しません。
ネット接続も問題なく、DSMだけ異常で、プロフィールを見ても問題なく、登録をやり直して承認されたメールアドレスを入力しても解決しません。
Just an example of the Fill patch with tangent command. Not of G2 surface continuity 'A' class quality, but under the hood or of everything other than high mirror gloss finish, perfectly adaquate but that's your decision and not mine to make.
If attempting this, be aware it takes a some practice to get proficient at surface modelling.
A less extreme patch with wider apart Y branches...
Note the reflections.
点我点这个的时候
出现了这个界面
当我点他的时候,又出现了这个界面
然而当我点这个的时候,又回到了第一张图片
我到底该怎么做
帮助我,谢谢:( When i try to start the DesignSpark a popup window says: "DesignSparkencountered an error during registration" , but i Swedish.
What shuld i do? In version 2 of Plasticity ( powerful Parasolid modeller) , X-nurbs is introduced for the premium Studio licence. X-nurbs is a fast professional tool having professional Lofting and Patching functionality with G1 and G2 surface continuity controls.
This YT contributor had problems with Plasticity current Indie licence to make the blend. Plasticity xNURBS for PRODUCT DESIGN Can Be Amazing! (youtube.com)
Here below is DSM v6 making the blend with accurate G1 Surface continuity. Surface curvature continuity ( G2) can be approached and approximated by moving the spline control points manually see below image - Explorer can do this!
For many shapes , DSM has sufficiant tools to do the job. Learn with DSM !
Below an automatic Patch fill with tangency - pink faces are a separate face.
Below is the rear face Patch filled with automatic tangency.
TIP: It only works because the pink surface is a separate surface - when patched, then combine the face to join. Tangency is very accurate to all edges.
For users of Creator and Engineer, simply use the Mirror Tool to make a mirror surface joining automatically. An option is to maintain mirror face relatationships or not.
Bonjour,
Je suis entrain de concepter des Pcb à plusiers couches dans DS PCB ENGINEER 11.0. Ma questions :
C'est quoi les paramètres essentiels pour concepter une Pcb ?
Par exemple est - ce que la couche de masse est obligatoire?
Merci d'avance
Translation by Moderator:
I'm designing multi-layer PCBs in DS PCB ENGINEER 11.0. My questions:
What are the essential parameters for designing a PCB?For example, is the mass layer mandatory?
how to highlight unconnected nets in PCB Login to PCB failed as it says "failed getting HArdwareid" Could not get Device ID
current version 11.0.1
PCB started as ADMIN
Local Firewal turned off
Network Firewall allows access to Licensing API
PCB is checking the credentials - if wrong a MSG appears - if correct the above happens
what to do next?New Posts
New Spectrum Analyser software for SDRplay SDR receivers
import OBJ(Explorer)
図面モードでの破断をジグザグ線に変更したい
Power/ Signal Tracks
Comment supprimer les couches - How to remove layers
clip with plane
LicenceSpring exception etc
起動するとエラー表示が出る
Y Pipe Tangent Patch Surfacing example.
如何下载这个软件
Can´t start the DS program, it crash direcly
Patch Surface 7 sided with tangency - Plasticity comparison.
L'essentiel dans la conception Pcb - The essentials in PCB design
how to highlight unconnected nets in PCB
Login Failed
Our forums
Software
Activist Engineering
Building our Air Quality Kit
- posts
- 16