How do you feel about this article? Help us to provide better content for you.
Thank you! Your feedback has been received.
There was a problem submitting your feedback, please try again later.
What do you think of this article?
Connectors are generally categorized into Board-to-Board or Board-to-Wire.
For Board-to-Board connectors, trying to transmit hundreds or thousands of signals between boards can result in breakage of connectors during mating. This is due to mounting multiple rigid connectors on the board.
There are 2 problems in the production process. High accuracy for making molding dies and equipment are required when producing super high-pin-count components as mechanical parts. Additionally, during the mass production process, the defective rate tends to rise and cost doesn’t match market needs.
Floating Board-to-Board connectors, which absorb alignment errors of the X/Y axis, solve these problems instantly.
The FX23 series by Hirose is a Floating Board-to-Board connector which not only can solve these structural problems but also has good high-speed transmission characteristics. Additionally, FX23 has both signal and power contacts.
Visit our online catalogue for further information.
FX23 was first selected (in 2014) to be used in supercomputer and network servers at American research institutes since it allows signal transmission for the 100-300pin range between boards by using multiple FX23 connectors.
After that, FX23 was also used in 5G base transmission stations. Use of FX23 then expanded to automobile, vehicle, mobility, factory automation equipment, and machine tools because it prevents electrical interruption by vibration or shock.
As IoT and Industry 4.0 spreads and the creation of “Connected Factories” increases rapidly, the latest industrial machines require high-speed transmission from 5 to 10Gbps.
It is difficult to make a connector which has both the function of floating and high-speed transmission at the same time. However, FX23 by Hirose achieves these and 8Gbps.
Application Examples
Supercomputers, network servers, 5G base transmission stations, navigation/infotainment for automobile, factory automation equipment, machine tools, etc.
Features of FX23
- Floating amount: X direction: ±0.6mm, Y direction:±0.6mm
- High-speed transmission capability (8+ Gbps)
- Hybrid power design (3A/pin x 4 lines), Signal contact 0.5A/pin, Power contact 3A/pin
- Supports 105℃ to meet automotive specifications
- Stacking Height:15~30mm/vertical
- FX23 has also Vertical connection type. (Right angle receptacle)
- FX23L is the low-profile type(Stacking Height 8,10,12mm)
Visit our online catalogue for further information.
FX23/23L are series in the FunctionMAX family.
It includes other floating and high-speed transmission connectors.
Please feel free to contact Hirose Electric co., ltd about the details.
In cases where the application will demand a high level of reliability, such as automotive, please contact a company representative for further information.