How do you feel about this article? Help us to provide better content for you.
Thank you! Your feedback has been received.
There was a problem submitting your feedback, please try again later.
What do you think of this article?
In this tutorial Massimo Banzi, shows us how to use our Arduinos for real life situations. This project shows us how to use a DC motor to spin a color wheel at different speeds. Massimo also teaches us how to use a mosfet transistor in order to protect the circuit from potential current spikes from the DC motor.
A DC motor is a simple electro-mechanical device, normally powered by a 9V battery, whereas Arduino can only provide up to 5V from its pins. The other issue is when an electric motor is turned off it can generate a spike of voltage that can damage the circuit. In this tutorial, an arduino controlled mosfet transistor is used as a gate to open and close a separate circuit, where the electric motor is wired to a 9V battery. Since the motor and the Arduino are on two separate circuits, the Arduino is protected from dangerous spikes.
The mosfet is controlled by a simple push-button, that tells the transistor to close the circuit between the battery and the motor, causing the motor to start spinning. The code is actually simpler than in previous tutorials, as reading a signal from the button and applying it back to the mosfet transistor is all that needs to be done.
You can find the previous tutorials here and subscribe to the upcoming Arduino video tutorials. As Massimo always says: build it, hack it and share it on the internet, because Arduino is you.