Skip to main content

Quick and Easy respirator mask

I designed this 3D printable face mask. It enables the use of household tissues (or other materials) as a filter.

It seems obvious that wearing some kind of mask is better than nothing, for the user and others. The problem is of course that there aren't enough of the 'proper' ones to go around and the government is concerned about recommending them for fear of increasing the demand for PPE that the NHS so badly need. It would take a long time to ramp up production of the certified N95 masks. That's where my idea came in. There is a fairly detailed explanation of it's key points in this link so I won't repeat that here.

https://www.myminifactory.com/object/3d-print-quick-and-easy-coronavirus-mask-respirator-117196

For it to truly help solve the problem it obviously needs to be mass produced rather than 3D printed. It would require minor modification to make it injection moldable. The different types of filter would also needs some degree of testing and validation. It would also need to be endorsed by the government.
 

Key points

Uses household tissues as the filter.

Large filter area. This reduces the flow rate per area and allows more layers (12 – 16) to be used, thus increasing filtration efficiency.

Comfortable because the only thing against your skin is the tissue.

Shaped to fit snugly around the nose to make a good seal

Everything you need is printed, apart from the filter itself. No need for rubber bands, elastic or shoelaces!

Adjustable side straps.

Only 15 grams of material (PLA) and 1 hour 8 mins to print.

 
I would like to gauge if there would be any interest in getting this into mass production?
benharker has not written a bio yet…