DesignSpark论坛
通过论坛区与其他 DesignSpark 会员自由交流。就产品、技术、软件和未来创新创建新的对话或加入现有的讨论。提供解决方案帮助他人,或者向全球志同道合的工程师网络提问,为自己遇到的技术问题寻找答案。
Bonjour,
Comment calculer la distance minimale entre deux pistes dans une Pcb qui contient uniquement deux connecteurs et des pistes pour faire le teste de diélectrique pour une tension de 1000V.
Bonjour,
C'est la quelle est la différence entre plan de masse et le coulée de cuivre dans un Pcb ?
Merci d'avance .
Moderator Translation:
what is the difference between ground plane and copper pour in a PCB? Bonjour,
C'est quoi la signification de ce trait bleu ?
Merci d'avance
Moderator - Translation:
What does this blue line mean?
Pozdrav
Na koji nacin mogu obnoviti pretplatu te izvrsiti uplat After creating the sketch, DSM automatically cuts out the surface for me. How to turn it off. It used to be enough to turn off the Enable Constraint based sketching option. now it doesn't work. Hello, I am a complete newbie to the program. Nevertheless, I created a CAD drawing of my project as part of my final thesis. Now I would like to insert this into my PowerPoint as a rotating object. Does the program offer me this option? I would then record it with OBS and then embed the video in the PowerPoint.TLDR:I need an automatic rotation of the CAD drawing When can the program be adapted for macOS? This is the best design program for Windows. But I switched to macOS. Hi, I can't find out how I can start to draw a line (or anyting) a spesific distance from another line (or object).
I'm drawing a house, and when I want to draw a window in the wall, I want to start 1000 mm from left and 500 mm from top of the wall. How can I start at this point.
So far I'm drawing lines (1000 from left and 500 from top) and then erase them after the window is finished.
I hope there is another way to do this? The AutoCad options do not appear in my File Options panel, how can I enable them?
Bonjour,
Comment mettre le plan de masse sur une Pcb de plusieur layers ?
Merci d'avance
Moderator Translation:
How to put the ground plane on a PCB of several layers? With a Creator or Engineer subscription, DesignSpark Circuit Simulator allows your simulations to run longer than 1 minute and upto 1 hour of server compute time.
We list some key reasons why you may need an extended simulation time:
Run electro-thermal transient simulations long enough for temperatures to reach steady-state, to verify reliability under real world operating conditions.
Allows compute-intensive simulations, such as switching power electronic circuits, to run as long as necessary for line and load transient response tests.
Monitor the behaviour of critical components to varying inputs over an extended time period, such as for vehicle drive-cycle simulations.
Check out the article at https://www.rs-online.com/designspark/what-does-more-than-1-minute-of-simulation-time-allow-you-to-do
With a Creator or Engineer subscription, DesignSpark Circuit Simulator allows your simulations to run longer than 1 minute and upto 1 hour of server compute time.
We list some key reasons why you may need an extended simulation time:
Run electro-thermal transient simulations long enough for temperatures to reach steady-state, to verify reliability under real world operating conditions.
Allows compute-intensive simulations, such as switching power electronic circuits, to run as long as necessary for line and load transient response tests.
Monitor the behaviour of critical components to varying inputs over an extended time period, such as for vehicle drive-cycle simulations.
Read all about it at https://www.rs-online.com/designspark/what-does-more-than-1-minute-of-simulation-time-allow-you-to-do
People have tuened to SDR receivers if they want to explore radio communications, propagation or interesting radio signals from round the world. SDRplay RSP receivers are a popular, UK manufactured choice with good customer service and support.
They cover 1kHz to 2GHz as a communications receiver when used in conjunction with free software supplied by SDRplay for Windows, MacOS, Linux and Raspberry Pi.
However thanks to Australian software developer Steve Andrew, they can also become excellent, calibrated spectrum analysers! Steve has just launched a new version of his Windows-based Spectrum Analyser software which includes a tracking generator.
There's a brand new Website with documentation and support information over on https://www.spectrumanalyser.co.uk/
HiI specifically bought a subscription to import OBJ files. But this feature never showed up.
What is the problem? 図面モードで破断にした時 破断面の線を直線からジグザグ線に変更しようと
ファイル→Design Sparkオプション→図面→一般→ラインスタイルのオプション→破断ビューのクリッピングエッジを変更しても変化有りません。知っている方が居られたら宜しくお願い致します。新论坛帖子
Distance entre les pistes
Pan de masse / coulée de cuivre - Copper Ground / Pour
Trait bleu - Blue Line
Kako mogu obnoviti pretplatu - Renew Subscriptions
automatic cutting of sketch surfaces
Rotate a 3D model for a presentation
When will it be available for macOS?
Start line a spesific distance from another line.
AutoCad Export Options
Mettre le plan de masse - Ground Plane
What does more than 1 minute of simulation time allow you to do?
What does more than 1 minute of simulation time allow you to do?
New Spectrum Analyser software for SDRplay SDR receivers
import OBJ(Explorer)
図面モードでの破断をジグザグ線に変更したい