Skip to main content

A thermal runaway refers to the overheating of a technical apparatus due to a self-reinforcing process that generates heat. This damage usually causes the destruction of the apparatus and often leads to a fire or explosion.
SCHURTER_ThermalRunaway_21_2e7eca3b7c7b0ea3012525501403eadd960b7266.jpg

What are the causes?
The causes of a thermal runaway are varied and often random in nature. However, the ever-higher power density in electronic wiring and the trend towards miniaturization are without a doubt of particular importance. More and more functions are packed in compact modules, which then also have a correspondingly high power consumption.

Even slightly excessive currents in power electronics with only a little power loss lead to elevated temperatures of approximately 200°C.

The possible consequences: damage or disconnection of surrounding components, damage to the printed circuit board structure or, in the worst case, the triggering of a fire.

Build up
With a power semiconductor (e.g. MOSFET) the drain-source transmission resistance increases with rising temperatures, when connected, which results in an increasing loss of power in the barrier layer. If the elements are not sufficiently cooled - the high power density permits cooling - the power loss output in the form of heat can no longer be sufficiently dissipated, which also increases the transmission resistance. This process escalates and ultimately leads to destruction of the component.

ThermalRunaway_EN_2_c866da8c5bb13fea63cad86d2322996e675da2be.jpg

Cause diagram for thermal runaway at an n-channel MOSFET

How to protect against a short circuit?
The cooling of a system must dissipate at least as much energy as it is supplied with. The overcurrent during a thermal runaway is too low to cause a conventional fuse to trip. In principle, thermal circuit breakers or PTCs would be used. But the products available for the assembly of an SMD printed circuit board are too complicated or completely unsuitable.

How can this be solved?
SCHURTER develops and manufactures SMD thermal fuses with the lowest possible internal resistance for power electronics of the highest packing density. They can be reflow-soldered at a maximum temperature of 260°C without opening. The temperature trigger is therefore around 210°C during operation. This corresponds to a range above normal component temperature ratings, but still below the limit to create serious consequences. The fuse opens with or without current flow depending on the temperature. Such irreversible thermal fuses are resistant to mechanical shock, vibration, thermal shock, temperature cycles and moisture. They are also qualified according to AEC-Q200.

SCHURTER_Infografik_Thermo_EN_2_25acbc375f3ef7909dc6ec3fa06995c73cee7eb6.jpg

The SCHURTER Group is a globally successful Swiss technology business. With our components ensuring the clean and safe supply of power, input systems for ease of use and sophisticated overall solutions, we impress our customers with agility and excellent product and service quality. We focus on industrial equipment, medical equipment, automotive, avionics and space, data and communication and energy.