DesignSpark论坛
通过论坛区与其他 DesignSpark 会员自由交流。就产品、技术、软件和未来创新创建新的对话或加入现有的讨论。提供解决方案帮助他人,或者向全球志同道合的工程师网络提问,为自己遇到的技术问题寻找答案。
Hi, I can't find out how I can start to draw a line (or anyting) a spesific distance from another line (or object).
I'm drawing a house, and when I want to draw a window in the wall, I want to start 1000 mm from left and 500 mm from top of the wall. How can I start at this point.
So far I'm drawing lines (1000 from left and 500 from top) and then erase them after the window is finished.
I hope there is another way to do this? The AutoCad options do not appear in my File Options panel, how can I enable them?
Bonjour,
Comment mettre le plan de masse sur une Pcb de plusieur layers ?
Merci d'avance
Moderator Translation:
How to put the ground plane on a PCB of several layers? With a Creator or Engineer subscription, DesignSpark Circuit Simulator allows your simulations to run longer than 1 minute and upto 1 hour of server compute time.
We list some key reasons why you may need an extended simulation time:
Run electro-thermal transient simulations long enough for temperatures to reach steady-state, to verify reliability under real world operating conditions.
Allows compute-intensive simulations, such as switching power electronic circuits, to run as long as necessary for line and load transient response tests.
Monitor the behaviour of critical components to varying inputs over an extended time period, such as for vehicle drive-cycle simulations.
Check out the article at https://www.rs-online.com/designspark/what-does-more-than-1-minute-of-simulation-time-allow-you-to-do
With a Creator or Engineer subscription, DesignSpark Circuit Simulator allows your simulations to run longer than 1 minute and upto 1 hour of server compute time.
We list some key reasons why you may need an extended simulation time:
Run electro-thermal transient simulations long enough for temperatures to reach steady-state, to verify reliability under real world operating conditions.
Allows compute-intensive simulations, such as switching power electronic circuits, to run as long as necessary for line and load transient response tests.
Monitor the behaviour of critical components to varying inputs over an extended time period, such as for vehicle drive-cycle simulations.
Read all about it at https://www.rs-online.com/designspark/what-does-more-than-1-minute-of-simulation-time-allow-you-to-do
People have tuened to SDR receivers if they want to explore radio communications, propagation or interesting radio signals from round the world. SDRplay RSP receivers are a popular, UK manufactured choice with good customer service and support.
They cover 1kHz to 2GHz as a communications receiver when used in conjunction with free software supplied by SDRplay for Windows, MacOS, Linux and Raspberry Pi.
However thanks to Australian software developer Steve Andrew, they can also become excellent, calibrated spectrum analysers! Steve has just launched a new version of his Windows-based Spectrum Analyser software which includes a tracking generator.
There's a brand new Website with documentation and support information over on https://www.spectrumanalyser.co.uk/
HiI specifically bought a subscription to import OBJ files. But this feature never showed up.
What is the problem? 図面モードで破断にした時 破断面の線を直線からジグザグ線に変更しようと
ファイル→Design Sparkオプション→図面→一般→ラインスタイルのオプション→破断ビューのクリッピングエッジを変更しても変化有りません。知っている方が居られたら宜しくお願い致します。 Bonjour,
Dans une Pcb le courant qui circule c'est entre 100 µA et 2 A .
Est ce que les pistes de class signal est suffisant?
Si non, comment je peux changer la classe liste des pistes pour avoir une class power?
Merci d'avance.
Moderators Translation:
Good morning,
In a PCB the current flowing is between 100 µA and 2 A.
Are class signal tracks sufficient?
If not, how can I change the track list class to have a power class?
Thanks in advance. Bonjour,
Est ce que cette Pcb contient 4 couches?
Si oui; comment je supprimer les autres 2 couches ?
Et qui est les couches qui sont pas utilisé pour le supprimé ?
Merci d'avance
Moderator translation:
Good morning,
Does this PCB contain 4 layers?
If yes; how do I remove the other 2 layers?
And which layers are not used for the deleted?
Thanks in advance I would like to create two objects from one,possibly with "clip with plane". I want an upper half and a lower half. can someone help? Morning, I restored a complete backup from my old (now defunct) laptop to a new laptop. DSPCB will not start and I get a message shown in the attachement below. Can anyone help please. (DSPCB still works perfectly on my main PC). Thanks in advance winodws10では正常に動作していましたが、windows11にアップグレートしてからは、DesignSpark Mechanicalを起動するとエラー表示してスタートしません。FAQを見ても1,2,3,5を確認しても解決しません。
ネット接続も問題なく、DSMだけ異常で、プロフィールを見ても問題なく、登録をやり直して承認されたメールアドレスを入力しても解決しません。
Just an example of the Fill patch with tangent command. Not of G2 surface continuity 'A' class quality, but under the hood or of everything other than high mirror gloss finish, perfectly adaquate but that's your decision and not mine to make.
If attempting this, be aware it takes a some practice to get proficient at surface modelling.
A less extreme patch with wider apart Y branches...
Note the reflections.
点我点这个的时候
出现了这个界面
当我点他的时候,又出现了这个界面
然而当我点这个的时候,又回到了第一张图片
我到底该怎么做
帮助我,谢谢:(新论坛帖子
Start line a spesific distance from another line.
AutoCad Export Options
Mettre le plan de masse - Ground Plane
What does more than 1 minute of simulation time allow you to do?
What does more than 1 minute of simulation time allow you to do?
New Spectrum Analyser software for SDRplay SDR receivers
import OBJ(Explorer)
図面モードでの破断をジグザグ線に変更したい
Power/ Signal Tracks
Comment supprimer les couches - How to remove layers
clip with plane
LicenceSpring exception etc
起動するとエラー表示が出る
Y Pipe Tangent Patch Surfacing example.
如何下载这个软件