How do you feel about this article? Help us to provide better content for you.
Thank you! Your feedback has been received.
There was a problem submitting your feedback, please try again later.
What do you think of this article?
The correction of a bad circuit can be difficult with conventional edge triggers because the error state cannot be selected precisely. That is the reason why modern oscilloscopes like the R&S®Scope Rider (125-9462) offer various digital triggers that are specialized to address specific problems.
T&M Solutions
A digital trigger is a very unique and innovative concept. The benefit of this is that you are actually triggering on the same waveform that you are viewing on the screen. This means that the sensitivity of the trigger circuit precisely matches that of the scope, as well as the noise, the raise time and all the other characteristics of the trigger circuit precisely match the scope. Therefore, there is essentially zero trigger jitter. More importantly, one can always trigger on any signal that can be viewed.
The specialized digital triggers from Rohde & Schwarz are extremely accurate because they directly access the acquired samples and support a large selection of trigger conditions. These permit targeted debugging of recurring development tasks. In addition to the standard settings, additional qualifiers such as >, <, = and ≠ are available to expand the scope of application. Most triggers can be used on both analog and digital channels.
Most Important Trigger Types
Below, a selection of specialized digital trigger types should be explained briefly. For a better understanding, some pictures were added in order to explain the specific functionality more clearly.
Width & glitch. The width trigger acts directly on the duration of a positive or negative pulse. Very short pulse widths are referred to as glitches. These triggers are used during the analysis of pulse width modulations, for example with rotary encoders. They are also important in the analysis of logic circuits where missing clock pulses can lead to very large pulse widths, or glitches can interfere with the circuit.
Timeout & interval. These two trigger modes expand the pulse width trigger functionality in two directions. The timeout trigger checks whether or not a pulse is followed by another pulse within a defined time window. The interval trigger checks the distance between two pulses of the same polarity. This makes it easy to find any missing clock pulses.
Pattern & state. The pattern trigger is used for measurements on parallel buses because it makes it possible to logically link pulse width triggers on multiple channels. The state trigger is different in that it references the pattern to a clock edge. Both triggers permit targeted isolation of complex circuit states, such as those that occur on parallel buses.
Data2Clock & setup-and-hold. The Data2Clock or setup-and-hold trigger checks two special timings on the data line as a function of the circuit clock pulse. A violation of these time relationships can easily perpetuate in logic circuits and must be avoided at all costs. This is critical for memory ports, for example.
Rise time. A faulty rise time for a signal can lead to timing problems during on/off switching operations of DC power supply units. These problems can easily be isolated using the rise time trigger. This trigger determines whether the level of a signal reaches a target threshold value within the defined time window.
Runt. A rise time that is too slow can lead to a runt, i.e. a pulse that is too low. The runt trigger can be used to define the lower and the upper pulse height limits as well as the pulse length limits. This makes it possible to specifically isolate metastable states in circuits.
Window. The window trigger checks whether the signal is inside or outside a defined voltage range. This check is performed with a time limit for timed segments. The window trigger is used to analyze voltage deviations in power supply units.
TV/video. The TV/video triggers represent a special class of triggers that resemble the protocol triggers. These triggers can be linked to specific components, such as the lines and frames of various video standards, including PAL, NTSC and HD 1080p.